Skip to main content
ABITT.1
Associate III
Sep 19, 2024 8:46 AM UTC
Solved

STM32F746 : SW not running well without debugger

Hi,

I designed a sw on STM32F746 with STM32CubeIDE.

Some functions work fine when I use the debugger (ST-LINK) but this same functions halts when I don't use the debugger !

I play se sequence hereafter :

 - run the sw using debugger : execution ok

- exit de debugger session into the STM32CubeIDE, the sw still running well

- disconnect physically the ST-LINK, the sw still running well

- reset my board, the functions halt before end execution !!! (others functions work fine)

 

Someone can help me, please ?

This topic has been closed for replies.
ABITT.1
ABITT.1Best answer
Associate III
Sep 19, 2024 1:32 PM UTC

Sorry for my sollicitation but I found the origin of my problem.
It's my delay procedure based on DWT who blocked some time.
I replaced with the HAL_Delay() and it work fine.

I've not understood why the debugger mask the problem and done that it work normally

 

This ticket can be closed

8 replies

Associate II
Sep 19, 2024 9:06 AM UTC

Hi,

We'd need more context.
Could you show us some code ? What are you trying to do ? Where does the code stops ?

ABITT.1
ABITT.1Author
Associate III
Sep 24, 2024 5:46 AM UTC

Hi SMarie,

 

I've resolved my problem, it was my wait who not work well.

 

thanks 

Andrew Neil
Super User
Sep 19, 2024 9:27 AM UTC

Provide some instrumentation which allows you to see what your code is doing when the debugger is not connected.

eg, UART, LEDs, etc ...

In particular, make sure that your Hard Fault handler, and any other error handler(s) give a clear clear indication when they "fire"

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ABITT.1
ABITT.1AuthorBest answer
Associate III
Sep 19, 2024 1:32 PM UTC

Sorry for my sollicitation but I found the origin of my problem.
It's my delay procedure based on DWT who blocked some time.
I replaced with the HAL_Delay() and it work fine.

I've not understood why the debugger mask the problem and done that it work normally

 

This ticket can be closed

Andrew Neil
Super User
Sep 19, 2024 1:41 PM UTC

@ABITT.1 wrote:

This ticket can be closed


You do that by marking the solution:

https://community.st.com/t5/community-guidelines/help-others-to-solve-their-issues/ta-p/575256

 


@ABITT.1 wrote:

Sorry for my sollicitation but I found the origin of my problem.
It's my delay procedure based on DWT who blocked some time.
I replaced with the HAL_Delay() and it work fine.

I've not understood why the debugger mask the problem and done that it work normally


To understand that, you'd need to give more detail - in particular, show your code

https://community.st.com/t5/community-guidelines/how-to-write-your-question-to-maximize-your-chances-to-find-a/ta-p/575228 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Andrew Neil
Super User
Sep 19, 2024 2:07 PM UTC

@ABITT.1 The post that you mark as the solution should be one which actually gives the solution!

That would be your post - not mine!

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.