Skip to main content
Visitor II
Jan 19, 2026 6:13 AM UTC
Solved

STM32F446 DAC DMA Callbacks Not Firing (HAL_DAC_ConvCpltCallbackCh2 / HalfCplt)

There have been a few posts on this forum with the same issue, but it seems the root cause is different to this post or (probably) this one.
I am using an Stm32f446re Nucleo, and trying to output a waveform from dac2 using dma and tim6. 

What I have tried so far:

 

  • Trigger is set to Timer 6 Trigger Out event.

  • DMA is configured in Circular Mode.

  • I'm calling HAL_DAC_Start_DMA(...)

  • Tried changing the data width to half word and word, neither worked.
  • Callback functions are correctly named and defined in main.c:

void HAL_DAC_ConvCpltCallbackCh2(DAC_HandleTypeDef *hdac) {
	HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_8);
}

void HAL_DAC_ConvHalfCpltCallbackCh2(DAC_HandleTypeDef *hdac) {
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, 1);
}

I want to be able to set a flag variable to start processing the next buffer.

I will paste the rest of my code, it includes a (buggy) sine wave table but I can fix that once the callbacks are handled properly. It is just something to send to the dac to see that it works on my scope.
You might notice that I am only using the bottom half of my DAC output, as the voltage seems to plateau at 1.9V, as if cutoff by an op amp or similar. This is when the output buffer is off, as when it is on a sine wave turns into an almost square wave. I have a feeling this indicates my DAC is fried.
Tangential issues aside, I mainly just want to fix the callbacks. Thank you in advance :)

/* USER CODE BEGIN Header */
/**
 ******************************************************************************
 * @file : main.c
 * @brief : Main program body
 ******************************************************************************
 * @attention
 *
 * Copyright (c) 2026 STMicroelectronics.
 * All rights reserved.
 *
 * This software is licensed under terms that can be found in the LICENSE file
 * in the root directory of this software component.
 * If no LICENSE file comes with this software, it is provided AS-IS.
 *
 ******************************************************************************
 */
/* USER CODE END Header */
/* Includes ------------------------------------------------------------------*/
#include "main.h"

/* Private includes ----------------------------------------------------------*/
/* USER CODE BEGIN Includes */
#include <math.h>
#include "arm_math.h"
/* USER CODE END Includes */

/* Private typedef -----------------------------------------------------------*/
/* USER CODE BEGIN PTD */

/* USER CODE END PTD */

/* Private define ------------------------------------------------------------*/
/* USER CODE BEGIN PD */
#define DMA_BUFFER_SIZE 1024
#define SAMPLE_RATE 48000
#define DAC_MID 1024

uint16_t dma_buffer[2 * DMA_BUFFER_SIZE];


#define TABLE_SIZE 1024


int16_t sine_table[TABLE_SIZE];
uint32_t phase_acc = 0;
uint32_t phase_step;

void init_sine_table(void)
{
 for (int i = 0; i < TABLE_SIZE; i++) {
 sine_table[i] = (int16_t)(1024 * arm_sin_f32(2.0f * PI * i / TABLE_SIZE));
 }

 phase_step = (uint32_t)((440.0f * TABLE_SIZE / SAMPLE_RATE) * (1ULL << 16));
}

void fill_sine(uint16_t *buf, int n)
{
 for (int i = 0; i < n; i++) {
 uint32_t index = (phase_acc >> 16) & (TABLE_SIZE - 1);
 int16_t s = sine_table[index];

 buf[i] = DAC_MID + s;

 phase_acc += phase_step;
 }
}


void HAL_DAC_ConvCpltCallbackCh2(DAC_HandleTypeDef *hdac) {
	HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_8);
}

void HAL_DAC_ConvHalfCpltCallbackCh2(DAC_HandleTypeDef *hdac) {
	HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, 1);
}
/* USER CODE END PD */

/* Private macro -------------------------------------------------------------*/
/* USER CODE BEGIN PM */

/* USER CODE END PM */

/* Private variables ---------------------------------------------------------*/
DAC_HandleTypeDef hdac;
DMA_HandleTypeDef hdma_dac2;

TIM_HandleTypeDef htim6;

UART_HandleTypeDef huart2;

/* USER CODE BEGIN PV */

/* USER CODE END PV */

/* Private function prototypes -----------------------------------------------*/
void SystemClock_Config(void);
static void MX_GPIO_Init(void);
static void MX_DMA_Init(void);
static void MX_DAC_Init(void);
static void MX_TIM6_Init(void);
static void MX_USART2_UART_Init(void);
/* USER CODE BEGIN PFP */

/* USER CODE END PFP */

/* Private user code ---------------------------------------------------------*/
/* USER CODE BEGIN 0 */

/* USER CODE END 0 */

/**
 * @brief The application entry point.
 * @retval int
 */
int main(void)
{

 /* USER CODE BEGIN 1 */

 /* USER CODE END 1 */

 /* MCU Configuration--------------------------------------------------------*/

 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();

 /* USER CODE BEGIN Init */

 /* USER CODE END Init */

 /* Configure the system clock */
 SystemClock_Config();

 /* USER CODE BEGIN SysInit */

 /* USER CODE END SysInit */

 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_DMA_Init();
 MX_DAC_Init();
 MX_TIM6_Init();
 MX_USART2_UART_Init();
 /* USER CODE BEGIN 2 */
 HAL_TIM_Base_Start_IT(&htim6);

// HAL_StatusTypeDef status;
 init_sine_table();
 fill_sine(&dma_buffer[0], DMA_BUFFER_SIZE);
 fill_sine(&dma_buffer[DMA_BUFFER_SIZE], DMA_BUFFER_SIZE);

HAL_DAC_Start_DMA(
 &hdac,
 DAC_CHANNEL_2,
 (uint32_t*)dma_buffer,
 2*DMA_BUFFER_SIZE,
 DAC_ALIGN_12B_R
);
 /* USER CODE END 2 */

 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
//	 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_8);
//	 HAL_Delay(1000);
 /* USER CODE END WHILE */

 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

/**
 * @brief System Clock Configuration
 * @retval None
 */
void SystemClock_Config(void)
{
 RCC_OscInitTypeDef RCC_OscInitStruct = {0};
 RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

 /** Configure the main internal regulator output voltage
 */
 __HAL_RCC_PWR_CLK_ENABLE();
 __HAL_PWR_VOLTAGESCALING_CONFIG(PWR_REGULATOR_VOLTAGE_SCALE1);

 /** Initializes the RCC Oscillators according to the specified parameters
 * in the RCC_OscInitTypeDef structure.
 */
 RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI;
 RCC_OscInitStruct.HSIState = RCC_HSI_ON;
 RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT;
 RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
 RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSI;
 RCC_OscInitStruct.PLL.PLLM = 8;
 RCC_OscInitStruct.PLL.PLLN = 180;
 RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV2;
 RCC_OscInitStruct.PLL.PLLQ = 2;
 RCC_OscInitStruct.PLL.PLLR = 2;
 if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
 {
 Error_Handler();
 }

 /** Activate the Over-Drive mode
 */
 if (HAL_PWREx_EnableOverDrive() != HAL_OK)
 {
 Error_Handler();
 }

 /** Initializes the CPU, AHB and APB buses clocks
 */
 RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK
 |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2;
 RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK;
 RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1;
 RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV4;
 RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV2;

 if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_5) != HAL_OK)
 {
 Error_Handler();
 }
}

/**
 * @brief DAC Initialization Function
 * None
 * @retval None
 */
static void MX_DAC_Init(void)
{

 /* USER CODE BEGIN DAC_Init 0 */

 /* USER CODE END DAC_Init 0 */

 DAC_ChannelConfTypeDef sConfig = {0};

 /* USER CODE BEGIN DAC_Init 1 */

 /* USER CODE END DAC_Init 1 */

 /** DAC Initialization
 */
 hdac.Instance = DAC;
 if (HAL_DAC_Init(&hdac) != HAL_OK)
 {
 Error_Handler();
 }

 /** DAC channel OUT2 config
 */
 sConfig.DAC_Trigger = DAC_TRIGGER_T6_TRGO;
 sConfig.DAC_OutputBuffer = DAC_OUTPUTBUFFER_DISABLE;
 if (HAL_DAC_ConfigChannel(&hdac, &sConfig, DAC_CHANNEL_2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN DAC_Init 2 */

 /* USER CODE END DAC_Init 2 */

}

/**
 * @brief TIM6 Initialization Function
 * None
 * @retval None
 */
static void MX_TIM6_Init(void)
{

 /* USER CODE BEGIN TIM6_Init 0 */

 /* USER CODE END TIM6_Init 0 */

 TIM_MasterConfigTypeDef sMasterConfig = {0};

 /* USER CODE BEGIN TIM6_Init 1 */

 /* USER CODE END TIM6_Init 1 */
 htim6.Instance = TIM6;
 htim6.Init.Prescaler = 5-1;
 htim6.Init.CounterMode = TIM_COUNTERMODE_UP;
 htim6.Init.Period = 375-1;
 htim6.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE;
 if (HAL_TIM_Base_Init(&htim6) != HAL_OK)
 {
 Error_Handler();
 }
 sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE;
 sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE;
 if (HAL_TIMEx_MasterConfigSynchronization(&htim6, &sMasterConfig) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN TIM6_Init 2 */

 /* USER CODE END TIM6_Init 2 */

}

/**
 * @brief USART2 Initialization Function
 * None
 * @retval None
 */
static void MX_USART2_UART_Init(void)
{

 /* USER CODE BEGIN USART2_Init 0 */

 /* USER CODE END USART2_Init 0 */

 /* USER CODE BEGIN USART2_Init 1 */

 /* USER CODE END USART2_Init 1 */
 huart2.Instance = USART2;
 huart2.Init.BaudRate = 115200;
 huart2.Init.WordLength = UART_WORDLENGTH_8B;
 huart2.Init.StopBits = UART_STOPBITS_1;
 huart2.Init.Parity = UART_PARITY_NONE;
 huart2.Init.Mode = UART_MODE_TX_RX;
 huart2.Init.HwFlowCtl = UART_HWCONTROL_NONE;
 huart2.Init.OverSampling = UART_OVERSAMPLING_16;
 if (HAL_UART_Init(&huart2) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN USART2_Init 2 */

 /* USER CODE END USART2_Init 2 */

}

/**
 * Enable DMA controller clock
 */
static void MX_DMA_Init(void)
{

 /* DMA controller clock enable */
 __HAL_RCC_DMA1_CLK_ENABLE();

 /* DMA interrupt init */
 /* DMA1_Stream6_IRQn interrupt configuration */
 HAL_NVIC_SetPriority(DMA1_Stream6_IRQn, 0, 0);
 HAL_NVIC_EnableIRQ(DMA1_Stream6_IRQn);

}

/**
 * @brief GPIO Initialization Function
 * None
 * @retval None
 */
static void MX_GPIO_Init(void)
{
 GPIO_InitTypeDef GPIO_InitStruct = {0};
 /* USER CODE BEGIN MX_GPIO_Init_1 */

 /* USER CODE END MX_GPIO_Init_1 */

 /* GPIO Ports Clock Enable */
 __HAL_RCC_GPIOC_CLK_ENABLE();
 __HAL_RCC_GPIOH_CLK_ENABLE();
 __HAL_RCC_GPIOA_CLK_ENABLE();
 __HAL_RCC_GPIOB_CLK_ENABLE();

 /*Configure GPIO pin Output Level */
 HAL_GPIO_WritePin(GPIOA, GPIO_PIN_8, GPIO_PIN_RESET);

 /*Configure GPIO pin : B1_Pin */
 GPIO_InitStruct.Pin = B1_Pin;
 GPIO_InitStruct.Mode = GPIO_MODE_IT_FALLING;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 HAL_GPIO_Init(B1_GPIO_Port, &GPIO_InitStruct);

 /*Configure GPIO pin : PA8 */
 GPIO_InitStruct.Pin = GPIO_PIN_8;
 GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP;
 GPIO_InitStruct.Pull = GPIO_NOPULL;
 GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW;
 HAL_GPIO_Init(GPIOA, &GPIO_InitStruct);

 /* USER CODE BEGIN MX_GPIO_Init_2 */

 /* USER CODE END MX_GPIO_Init_2 */
}

/* USER CODE BEGIN 4 */

/* USER CODE END 4 */

/**
 * @brief This function is executed in case of error occurrence.
 * @retval None
 */
void Error_Handler(void)
{
 /* USER CODE BEGIN Error_Handler_Debug */
 /* User can add his own implementation to report the HAL error return state */
 __disable_irq();
 while (1)
 {
 }
 /* USER CODE END Error_Handler_Debug */
}
#ifdef USE_FULL_ASSERT
/**
 * @brief Reports the name of the source file and the source line number
 * where the assert_param error has occurred.
 * file: pointer to the source file name
 * line: assert_param error line source number
 * @retval None
 */
void assert_failed(uint8_t *file, uint32_t line)
{
 /* USER CODE BEGIN 6 */
 /* User can add his own implementation to report the file name and line number,
 ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */
 /* USER CODE END 6 */
}
#endif /* USE_FULL_ASSERT */

 

Saket_OmBest answer
ST Technical Moderator
Jan 19, 2026 9:14 AM UTC

Hello @sinkspaghetti 

For DMA + Channel 2, the callbacks are not the generic HAL_DAC_ConvCpltCallback but the channel‑specific ones:

  • HAL_DACEx_ConvCpltCallbackCh2
  • HAL_DACEx_ConvHalfCpltCallbackCh2
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om

1 reply

Saket_OmBest answer
ST Technical Moderator
Jan 19, 2026 9:14 AM UTC

Hello @sinkspaghetti 

For DMA + Channel 2, the callbacks are not the generic HAL_DAC_ConvCpltCallback but the channel‑specific ones:

  • HAL_DACEx_ConvCpltCallbackCh2
  • HAL_DACEx_ConvHalfCpltCallbackCh2
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om