Skip to main content
Associate
Nov 21, 2024 7:23 AM UTC
Solved

STM32CubeMX file for the STM32H747I_DISCO_USB_Webcam example?

I want to make some modifications to the STM32H747I_DISCO_USB_Webcam example embedded in the FP-AI-VISION1 package, however I cannot find a way to open it in STM32CubeMX. I also checked the repository on GitHub for this example and no success. Any idea about how to open the settings of this example in STM32CubeMX?

 

Thanks!

This topic has been closed for replies.
Andrew Neil
Andrew NeilBest answer
Super User
Nov 21, 2024 9:52 AM UTC

You mean a .ioc file?

Not all examples have a .ioc file:

https://community.st.com/t5/stm32-mcus-products/some-example-projects-don-t-use-ioc-file/m-p/698338/highlight/true#M255312

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

3 replies

Andrew Neil
Andrew NeilBest answer
Super User
Nov 21, 2024 9:52 AM UTC
A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Associate
Nov 21, 2024 9:55 AM UTC

Got it. If I understood correctly I might need to export all the settings manually in STM32CubeMX then.

Andrew Neil
Super User
Nov 21, 2024 9:57 AM UTC

So there is no CubeMX project - if you want one, you're going to have to create it yourself based on the settings in the code.

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.