Skip to main content
Associate III
July 7, 2025
Question

Standby and Shutdown mode in stm32u585 using RTC

Hi,

  I am on stm32u585 IOT dev board for low power modes am using RTC wakeup the sleep and stop 1,2 and 3 are working fine but standby and shutdown is not working ? my code 

 
void sleep(int mode, int seconds ) {

if (seconds <= 0) return;

 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);

 __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);

uint32_t wakeup_counter (uint32_t)(seconds 2048);

 HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, wakeup_counter, RTC_WAKEUPCLOCK_RTCCLK_DIV16, 0);




switch (mode) {

case 0: // Sleep

 HAL_SuspendTick();

HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);

 HAL_ResumeTick();

break;

case 1: // Stop0

 HAL_SuspendTick();

 HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);

break;

case 2: // Stop1

 HAL_SuspendTick();

 HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);

break;

case 3: // Stop2

 HAL_SuspendTick();

 HAL_PWREx_EnterSTOP3Mode(PWR_STOPENTRY_WFI);

break;

case 4: // Standby

 __HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_ALL_FLAG | PWR_FLAG_SBF);

 HAL_PWR_EnterSTANDBYMode();

break;

case 5; // Shutdown/DeepSleep

 __HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_ALL_FLAG | PWR_FLAG_SBF);

 HAL_PWREx_EnterSHUTDOWNMode();

break;

default:

break;

 }

}

void HAL_RTCEx_WakeUpTimerEventCallback(RTC_HandleTypeDef *hrtc) {

 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);

 SystemClock_Config();

 HAL_ResumeTick();
}

 

10 replies

ST Technical Moderator
July 8, 2025

Hello @shivss 

The device cannot enter on standby and shutdown mode or cannot exit? 

Please refer to the example below: 

STM32CubeU5/Projects/NUCLEO-U545RE-Q/Examples/PWR/PWR_STANDBY at main · STMicroelectronics/STM32CubeU5 · GitHub

Note that The RTC remains active when the RTC clock source is LSE or LSI.

Saket_Om_0-1751971126551.png

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
shivssAuthor
Associate III
July 8, 2025

Hi,

It is not exit from standby and shutdown modes. The example code is using Wakeup pin but want I need is wakeup with RTC .In RTC INIT checking for wakeup same as in example . This code is working for sleep,stop1,2 and 3 the RTC is working fine  with these modes but not for standby or shutdown even UART messages are also not printing after standby or shutdown

static void MX_RTC_Init(void)
{

 /* USER CODE BEGIN RTC_Init 0 */
	uart_send("RTC start\r\n");
	// Check if waking from Standby — if yes, skip full init
	 if (__HAL_PWR_GET_FLAG(PWR_FLAG_SBF) != RESET)
	 {
		 uart_send(">> Woke from STANDBY\r\n");
	 __HAL_PWR_CLEAR_FLAG(PWR_FLAG_SBF); // Clear standby flag

	 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);
	 }

 /* USER CODE END RTC_Init 0 */

void sleep(int mode, int seconds ) {

if (seconds <= 0) return;

 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);

 __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);

uint32_t wakeup_counter (uint32_t)(seconds 2048);

 HAL_RTCEx_SetWakeUpTimer_IT(&hrtc, wakeup_counter, RTC_WAKEUPCLOCK_RTCCLK_DIV16, 0);




switch (mode) {

case 0: // Sleep

 HAL_SuspendTick();

HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);

 HAL_ResumeTick();

break;

case 1: // Stop0

 HAL_SuspendTick();

 HAL_PWREx_EnterSTOP1Mode(PWR_STOPENTRY_WFI);

break;

case 2: // Stop1

 HAL_SuspendTick();

 HAL_PWREx_EnterSTOP2Mode(PWR_STOPENTRY_WFI);

break;

case 3: // Stop2

 HAL_SuspendTick();

 HAL_PWREx_EnterSTOP3Mode(PWR_STOPENTRY_WFI);

break;

case 4: // Standby

 __HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_ALL_FLAG | PWR_FLAG_SBF);

 HAL_PWR_EnterSTANDBYMode();

break;

case 5; // Shutdown/DeepSleep

 __HAL_PWR_CLEAR_FLAG(PWR_WAKEUP_ALL_FLAG | PWR_FLAG_SBF);

 HAL_PWREx_EnterSHUTDOWNMode();

break;

default:

break;

 }

}

void HAL_RTCEx_WakeUpTimerEventCallback(RTC_HandleTypeDef *hrtc) {

 HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);

 SystemClock_Config();

 HAL_ResumeTick();
}

 Screenshot 2025-07-08 182837.png

Hai
ST Employee
July 8, 2025

Hello @shivss 

Could you please ensure that the RTC wake-up timer interrupt is properly configured by adding the following functions ? Once done, kindly let us know if the issue persists:

 /* Enable WakeUp line functionality for the RTC ALARMA */
 HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN7_HIGH_3);

 /* Enable the Autonomous Mode for the RTC */
 __HAL_RCC_RTCAPB_CLKAM_ENABLE();

Best regards,

Haifa.

shivssAuthor
Associate III
July 9, 2025

Hi @Hai 

 
HAL_RTCEx_DeactivateWakeUpTimer(&hrtc);

/*functionality for the RTC ALARMA */
 HAL_PWR_EnableWakeUpPin(PWR_WAKEUP_PIN7_HIGH_3);

 /* Enable the Autonomous Mode for the RTC */
 __HAL_RCC_RTCAPB_CLKAM_ENABLE();

 __HAL_RTC_WAKEUPTIMER_CLEAR_FLAG(&hrtc, RTC_FLAG_WUTF);/* Enable WakeUp line 

I have added after the deactivate wakeup timer  then it wakeup one time after then when am trying to send it again back to standby/shutdown then its not even entering into standby/shutdown its getting hang   

shivssAuthor
Associate III
July 13, 2025

Hi @Hai 

 Waiting the reply with solution . Thanks

shivssAuthor
Associate III
July 29, 2025

HI ,

any reply ? can you guys give me example code for all sleep ,stop and shutdown and standby ? or any working code

ST Technical Moderator
July 30, 2025
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
shivssAuthor
Associate III
July 30, 2025

HI @Saket_Om 

 

That is for different board and more over that is not standby or shutdown mode?

Visitor II
November 27, 2025

Hello @shivss 
Were you able to solve the problem?

NFern.1
Associate III
February 16, 2026

Hi @shivss @pyszny 

Could you figure out the correct configuration to wake-up from Shut-down using RTC Alarm for U5x MCUs? Please share your solution if possible. Thanks!