Skip to main content
Associate
Mar 11, 2024 7:33 PM UTC
Solved

PSSI_Transmit_Receive_DMA example does not work

Hello,

I used two nucleo-H723ZG boards to try the PSSI_Transmit_Receive_DMA example code in the STM32Cube\Repository\STM32Cube_FW_H7_V1.11.1\Projects\NUCLEO-H723ZG\Examples\PSSI directory, the LEDs on both boards do not flash as expected (master board, the LED2 stayed on all the time, and the 3 LEDs on the slave board never turned on).  I followed the instructions in the readme.txt to setup the boards and build the example software.  The only issue that I found in the readme.txt is the identification of PC8 pin wrong, instead as stated "CN12 PIN10", it shall be CN12 PIN3 for the STM32H723 MCU.

Any suggestions to get the example code running on the two boards?

 

Thank you in advance.

 

Patrick

This topic has been closed for replies.
Imen.DBest answer
ST Technical Moderator
Mar 20, 2024 9:22 PM UTC

Hello @patricky30,

I would inform you that this issue is fixed in the new release of STM32CubeH7 (v1.11.2)

Thank you for your contribution.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks

4 replies

ST Technical Moderator
Mar 11, 2024 8:34 PM UTC

Hello @patricky30 and welcome to the Community :) 

I invite you to follow this FAQ: How to configure and use the PSSI on the STM32H7, this may help you.

Thank you for your contribution.

 

 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Associate
Mar 13, 2024 4:48 PM UTC

Figured it out.  Need to make the following changes:

1. Change to: hdma_handler_tx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;.

2. Change to: hdma_handler_rx.Init.FIFOMode = DMA_FIFOMODE_ENABLE;

3. Change to:

__IO uint32_t PSSI_HAL_PSSI_TransmitComplete_count = 0;
__IO uint32_t PSSI_HAL_PSSI_ReceiveComplete_count = 0;
__IO uint32_t PSSI_HAL_PSSI_ErrorCallback_count = 0;

Hope STMicroelectronics will make the changes in their next updated package.

Thanks.

Patrick

 

ST Technical Moderator
Mar 13, 2024 8:45 PM UTC

Hi @patricky30 ,

Thanks for sharing this issue and the solution!

An internal ticket number 176023 is submitted in order to fix this.

(PS: 176023 is only for reference and not available outside of ST)

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks
Imen.DBest answer
ST Technical Moderator
Mar 20, 2024 9:22 PM UTC

Hello @patricky30,

I would inform you that this issue is fixed in the new release of STM32CubeH7 (v1.11.2)

Thank you for your contribution.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Thanks