Skip to main content
Ehab
Visitor II
Jan 18, 2021 2:18 PM UTC
Question

Microcontroller requirements to implement an embedded web server using WebSocket, JS, and HTML5

Hi,

I'm developing a new product, and one of the design requirements is to implement an embedded web server on the microcontroller. The web pages should be responsive and dynamic like single page application (SPA) web pages and there are 3 pages to be implemented with light images and graphics.

I plan to pick out a microcontroller from the STM32 range, and my questions are related to the hardware design part :

  1. what are the minimum Microcontroller requirements to implement an embedded web server in terms of performance and memory?
  2. what is the approximate size of the used memory for the lwIP stack, web server, and client-side code?
  3. where to store the webpages? internal Flash, ROM, External Flash?
  4. And finally, what is the complexity level of the implementation in comparison to the traditional HTTP request?

Thanks,

This topic has been closed for replies.

18 replies

TDK
Jan 18, 2021 2:42 PM UTC

That sounds significantly above the capabilities of any STM32 MCU. I'm sure one of the STM32MP chips could do it, or a RPi.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Piranha
Principal III
Jan 20, 2021 4:47 PM UTC

The reality is almost the exact opposite. ;) Any STM32 with Ethernet can do at least the minimum of those requirements. Read more information in my other comment.

Tesla DeLorean
Guru
Jan 18, 2021 5:33 PM UTC

Doing simple page serving is one thing, expecting all kinds of other packages to be available and readily integrated is another. Data and graphics provided it is not too large can fit in internal memory, ST has parts with 1MB and 2MB of FLASH readily available. External QSPI memories can easily add up to 256 MB, although the sweet spot for parts is probably 16 or 32 MB.

Look at what commercial stack vendors offer on MCU's and if that meets your time/budget requirements. Otherwise build a model in Embedded Linux and see just how involved that gets.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Piranha
Principal III
Jan 20, 2021 4:44 PM UTC

I have a project, where I'm doing almost exactly the same thing - dynamically (with snprintf() style function) building HTML, serving static CSS and JS files (directly linked in with linker script), and using AJAX for bidirectional data exchange. The project currently takes 80 KB of ROM, about the same size of RAM and it's already pretty packed with features and besides network related parts has a few other non-trivial software modules.

The lwIP stack itself will take 40-60 KB ROM and similar but even wider range of RAM sizes, depending on configuration. Therefore the approximate minimum requirement for a MCU is 128 KB of ROM and 64 KB of RAM, which means that any STM32 with Ethernet can do it (even STM32F107RB). If up to 2 MB of ROM is enough for everything, go for internal FLASH, if not, add some external QSPI memory. For a basic network servicing the CPU speed doesn't matter much - it mostly depends on what processing and data traffic amounts the application requires.

Of course, for all that to be possible, the software has to be sanely designed. The lwIP stack itself is pretty robust. It's HTTPd web server is of average quality. Nonetheless I managed to get even POST requests for AJAX working with it. It's not trivial, but it's not an impossible magic either. But one thing is for sure - it's not possible to do this by clicking CubeMX.

P.S. Take a look on my demonstration firmware for the network part:

https://community.st.com/s/question/0D50X0000AhNBoWSQW/actually-working-stm32-ethernet-and-lwip-demonstration-firmware

waclawek.jan
Super User
Jan 21, 2021 12:27 AM UTC

> responsive and dynamic

What's that?

> And finally, what is the complexity level of the implementation in comparison to the traditional HTTP request?

Imagine a PC without AMP or similar stack. All you have is TCP/IP stack, and you have to write the rest.

As Piranha said, there's a HTTP server in lwip, but it's quite rudimentary (if you compare it to Apache and kin), and to expand on it - or even use it as it is now - means to dig relatively deep into it. At the end of the day you'll feel like rewriting it from scratch.

But why don't you try? The basic LWIP demo will probably run on any Nucleo144 board which has Ethernet (never tried myself, but started with a 'F4 EVAL back then).

JW

Jack Peacock_2
Associate II
Jan 21, 2021 2:24 AM UTC

Your requirements point towards using one of the )too numerous to count) Cortex A series application processors. These are built specifically to handle the kinds of tasks you describe, plus about 90% of the software (i.e. Linux) is already done and well tested. One big advantage to going with an A series is that if a single core proves too slow you can drop in a two or four core replacement without a PCB redesign.

Worst case you might look at the dual core A7/M4 variants in the STM32 line. There are other vendors who specialize in A series with much broader lines than ST. If your technical resources are limited to M series controllers, and you don't want to buy (very cheap) A series boards this is likely the best place to start.

Think of it this way: theoretically you can cross the ocean in a rowboat, but it's a lot faster, cheaper and less complicated in a plane. Part of the design process is selecting the right tool for the job.

Jack Peacock

clock.1166
Senior
Oct 3, 2021 9:04 AM UTC

Hi Ehab,

I'm going up the learning curve for a very similar project.

I've chosen STM32H743ZI2 and LWIP/RTOS.

I'm wondering whether this is the right solution?

Could you tell me what hardware you finally decided upon?

Thanks,

Chris

clock.1166
Senior
Oct 3, 2021 9:23 AM UTC

Or could anyone else give an opinion?

Thanks,

Chris

waclawek.jan
Super User
Oct 3, 2021 10:07 AM UTC

As I've said, get the Ethernet enabled Nucleo144 and try yourself.

JW

clock.1166
Senior
Oct 3, 2021 10:37 AM UTC

I've already got the hardware - I just want to know whether the above board is the right choice

for 3 small web pages as per Ehabs post or should I choose a different variant?

I have the LWip/netconn/rtos demo working, but it seems very complex (for me anyway).

I dont want to spend weeks on it and find that I should have chosen a different solution.

Chris

Pavel A.
Oct 3, 2021 11:09 AM UTC

Check your requirements. If the client will have a decent browser that supports client side scripts, decompression (for static files), web sockets or fetch, STM32 MCUs may be capable to serve few clients.

> I dont want to spend weeks on it

Unfortunately, this is *at least* the expected time for such project om STM32 MCU. Unless you find somebody with a ready prototype.

clock.1166
Senior
Oct 3, 2021 11:30 AM UTC

Thanks, but 'STM32 MCUs may be capable to serve few clients.'.... Which ones are most suited?

Should I continue with STM32H743?

Can anyone help me with a ready prototype?

I'm quite willing to spend time and money - I just need direction.

As I've said, I am not as experienced as most of the contributors here in- 'client side scripts, decompression (for static files), web sockets or fetch,'........

but I'm also willing to learn.

Thanks,

Chris

Pavel A.
Oct 3, 2021 2:18 PM UTC

> Should I continue with STM32H743?

Let's see. As you already know, there's a problem with ordering. Do you have H743 in stock?

H743 has 2 MB of internal flash. This can be enough for the code, but for website data you may need external memory.

What kind of network connection do you want?

H743 has only plain ethernet. For wi-fi or cellular you will need external chips/modules.

On the other hand, you can connect a WIZnet to any other MCU without ethernet controller, and it will even do TCP/IP.