Skip to main content
Ehab
Visitor II
Jan 18, 2021 2:18 PM UTC
Question

Microcontroller requirements to implement an embedded web server using WebSocket, JS, and HTML5

Hi,

I'm developing a new product, and one of the design requirements is to implement an embedded web server on the microcontroller. The web pages should be responsive and dynamic like single page application (SPA) web pages and there are 3 pages to be implemented with light images and graphics.

I plan to pick out a microcontroller from the STM32 range, and my questions are related to the hardware design part :

  1. what are the minimum Microcontroller requirements to implement an embedded web server in terms of performance and memory?
  2. what is the approximate size of the used memory for the lwIP stack, web server, and client-side code?
  3. where to store the webpages? internal Flash, ROM, External Flash?
  4. And finally, what is the complexity level of the implementation in comparison to the traditional HTTP request?

Thanks,

This topic has been closed for replies.

18 replies

waclawek.jan
Super User
Oct 3, 2021 1:06 PM UTC

> Should I continue with STM32H743?

This of course depends on what do you want to achieve exactly. Is there any "controller" (hard real time) side to the project, or do you want to use the STM32 simply as a suitable "small computer"? Is the web-side of the project to be fancy, or is flat HTML OK? What is the expected "other side" (i.e. network and browser issues)?

I don't offer help here, I'm just merely saying that these are probably the most basic questions for which you have to have very clearly formulated answers prior to talking to anybody for further help.

You may want to have a look at/post on the lwip users mailing list, too.

JW

clock.1166
Senior
Oct 3, 2021 3:23 PM UTC

Thanks all for the info.

I just thought that I would have more control over the whole thing if I used a microcontroller and also I would learn a lot more.

I have several H743 boards.

I dont need wifi or cellular, just a LAN connection.

I can see that it may be easier using a Pi, but then you have the whole complication of a big O/S to consider.

Surely, it would be simpler to use an STM32 board?

However, the wiznet device looks interesting - I will check that out.

I presume that you could then use a low level F103 type board?

Chris

Piranha
Principal III
Oct 10, 2021 8:06 PM UTC

My previous post answers all of your questions...

clock.1166
Senior
Oct 11, 2021 7:29 AM UTC

Thanks everybody. Everything I appear to need is present in the project 'LwIP_HTTP_Server_Netconn_RTOS', and I

am finding this very difficult to understand, especially as my 'C' needs brushing up, - but I am slowly getting there.

Unlike most of you, I knew hardly anything about ethernet 3 months ago, so you may think that my questions

are somewhat simple!!

I am going to investigate the wiznet area as well.

My ultimate objectives are to gain knowledge and to have a cheaply produced

web server that will run the above project.

Chris