Skip to main content
Associate
Dec 13, 2024 11:09 AM UTC
Question

How to use ST Open bootloader for STM32L562ZET6Q

Moved from the Feedback Forum


Hi,

1. Referring to below link, can we use this for STM32L562ZET6Q part without any change.

2. What changes are to be done to make use of USART3 (PC10,PC11) rather USART1 (PA9,PA10).

 

How to use the ST Open Bootloader for STM32 Microc... - STMicroelectronics Community

This topic has been closed for replies.

11 replies

ST Technical Moderator
Dec 13, 2024 2:39 PM UTC

Hello @priyanka.yadav 

To be able to use the UART3 instead of UART1 you should update the lines below in the file interfaces_conf.h.

#define USARTx USART1

#define USARTx_TX_PIN GPIO_PIN_9
#define USARTx_TX_GPIO_PORT GPIOA
#define USARTx_RX_PIN GPIO_PIN_10
#define USARTx_RX_GPIO_PORT GPIOA
#define USARTx_ALTERNATE GPIO_AF1_USART1

s 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Associate
Dec 16, 2024 9:05 AM UTC

Hello @Saket_Om ,

Following changes have been made in code, but not connecting to desired UART.

priyankayadav_0-1734339933347.png

 

ST Technical Moderator
Dec 16, 2024 9:22 AM UTC

Hello @priyanka.yadav 

Could you provide more details about your setup please?

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
ST Employee
Dec 23, 2024 1:10 PM UTC

Hello @priyanka.yadav ,

Could you please check your bootloader version. if it is V13.0, according to AN2506 table 164, the USART3 is not working.

With regards

"If your question is answered, please close this topic by clicking ""Accept as Solution"""
Associate
Dec 24, 2024 8:44 AM UTC

Hello SirineST,

Bootloader version is showing as 0x92. Please see the snapshot.

Also, please note that USART3 is working when I'm trying to flash via USART3 (but only issue is that this requires manual intervention to uncheck nBOOT0 via ST-LINK debugger). So this is not IAP where we can fully program device via USART.

We are looking for solution where device initially waits for some timeout for data from usart and when its timeout then device will simply boot via flash. In this case if we don't wish to flash it'll simply boot via flash and in case we need to do IAP then we can stop and flash new file during timeout when its waiting for data from USART for any updated file.

Thanks!