Skip to main content
Associate II
Feb 13, 2025 9:50 AM UTC
Question

How to display the uart data on stm32f429i eval board?

Hello ST,

 I'm trying  to display the uart data on stm32f429i(MB1046) eval board GUI, followed below link as 

https://controllerstech.com/touchgfx-5-data-from-uart-to-ui/,

 
void HAL_UARTEx_RxEventCallback(UART_HandleTypeDef *huart, uint16_t Size)

{

RxData[Size] = '\0';

if (osMessageQueueGetSpace(uartQueueHandle)>0)

{

strncpy (uartData_q->Data, (char *)RxData, Size+1);

uartData_q->size = Size+1;

osMessageQueuePut(uartQueueHandle, &uartData_q, 0, 0);

HAL_UART_Transmit(&huart1, uartData_q->Data,uartData_q->size , 1000);

}

HAL_UARTEx_ReceiveToIdle_IT(&huart1, RxData, 256);

}

void StartDefaultTask(void *argument)

{

/* USER CODE BEGIN 5 */

HAL_UARTEx_ReceiveToIdle_IT(&huart1, RxData, 256);



/* Infinite loop */

for(;;)

{

osDelay(1000);

}

/* USER CODE END 5 */

}

This code added in main.c but uart  receive interrupt is not working.

could you please help me to develop.


Thanks& Regards,

PSR.

This topic has been closed for replies.

15 replies

Andrew Neil
Super User
Feb 13, 2025 10:01 AM UTC

Please see How to insert source code.

 

@PSR1 wrote:

code added in main.c but uart  receive interrupt is not working..


Before getting into the extra complications of interrupts, have you proved basic connectivity with a simple polled read?

Do this first in a standalone project - no TouchGFX.

https://wiki.st.com/stm32mcu/wiki/Getting_started_with_UART

https://wiki.st.com/stm32mcu/wiki/STM32StepByStep:Step3_Introduction_to_the_UART

https://community.st.com/t5/stm32-mcus/implementing-uart-receive-and-transmit-functions-on-an-stm32/ta-p/694926 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
PSR1Author
Associate II
Feb 13, 2025 10:18 AM UTC

Hello Andrew Neil,

Thanks for supporting, as you mentioned i have done but the i'm facing the issue as to integrate the touch gfx designer generated FREERTOS code, 

HAL_UART_Transmit(&huart1, TxData, 256 , 1000);

i added above line in main.c , The TxData is showing on teraterm.

 

Thanks & Regards,

PSR.

Andrew Neil
Super User
Feb 13, 2025 10:31 AM UTC

So you have confirmed that both Tx & Rx work in a simple standalone project without TouchGFX or FreeRTOS?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.