Skip to main content
Peter Curtis
Associate II
May 20, 2022 1:24 PM UTC
Question

How do you configure a PHY not listed in the LWIP platform settings?

Hi All,

I'm a long time user/developer of STM32 micros (on STM32IDE) but until now have managed to avoid anything ethernet. However, I couldn't avoid it forever and work have tasked me with a fairly urgent project.

I plan to design a custom board around the STM32H742 (which I have a few of from another project) coupled with an ethernet PHY running FreeRTOS (which I have some experience in) and LWIP. My original design used the LAN8742 (which is listed in the LWIP platfrom settings), but these aren't available until the middle/end of next year which doesn't meet the project timescales. So I need to find something else.

My question is:- If only the LAN8742 is listed in the LWIP platform settings, is it possible to use/configure a different PHY in CUBEMX/CUBEIDE? STM32CUBEIDE also tells me that it will select the LAN8742 as default if there is only one device listed (which there is), so how would/can I get around that?

Any help would/pointers would be very much appreciated at this point.

Kind regards,

Peter

This topic has been closed for replies.