STM32H745 not works with KSZ8081RNA
- 9 replies
- 6168 views
Hello!
I am trying to run ping on my board with STM32H745 (similar to NUCLEO-H745ZI-Q). Instead of the standard LAN8742, I have to use KSZ8081RNA. On the advice of @Piranha and @Pavel A. in other branches, I leave almost everything as it is in the LAN8742.c driver, I change only some registers in order for initialization to be successful (I only needed to change the LAN8742_GetLinkState function). I can read and write KSZ8081RNA registers. I see in debugging a link change when connecting/disconnecting an ethernet cable.
But ping data packets (ICMP) are still not coming to me.
The program does not pass /* Check if descriptor is not owned by DMA */ check (HAL_ETH_Read Data in the file stm32h7xx_hal_et.c line 1063) due to the values of the descriptors heth->RxDescList.RxDesc. It is equal to 0x81000000. In another, working project, it is equal to 0x3401003С.
Most likely, I did not fully initialize correctly, because the same project worked on NUCLEO-H745ZI-Q before the changes. I don't fully understand how packets are received via DMA. But what should I change except LAN8742_Init function?