Skip to main content
lChen.12
Associate
Mar 1, 2023 10:07 AM UTC
Question

Has the HAL library of STM32 been validated by the medical system,such as IEC 62304

Has the HAL library of STM32 been validated by the medical system,such as IEC 62304

This topic has been closed for replies.

5 replies

ST Employee
Mar 1, 2023 10:14 AM UTC

Hello @lChen.1​ and welcome to ST Community,

As mentioned in this thread, some validation reports are available for the STM32Cube HAL & LL drivers. You need to get in contact with your FAE to get them as they are delivered only under a non disclosure agreement "NDA".

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
lChen.12
lChen.12Author
Associate
Mar 1, 2023 10:18 AM UTC
  • I don't know my FAE. How should I contact him

My main objective was to find out if the HAL library passed IDE62304 validation

ST Employee
Mar 1, 2023 12:21 PM UTC

Hello again @AIcha.1​,

I escalated your request internally, you will be contacted soon

Thank you.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
Mar 1, 2023 1:38 PM UTC

Can't you run some basic static analysis tools to audit the code/library?

Do a code walk using your own rules and processes?

I'd be seriously uncomfortable using this on life safety critical spaces.

Most people who take this seriously develop their own curated code/library because ST's surely not going to indemnify you.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Piranha
Principal III
Mar 6, 2023 12:56 AM UTC

If I can point to hundreds of bugs in HAL right away with a finger without even testing, then such a software is terribly broken. The bloat, code style, architecture, development process and testing is also terrible. If it [Edit] can be validated as anything "safe" or even "fine", then it just shows how useless such a validation is!