Skip to main content
MOtto.1
Associate III
Jan 24, 2022 8:20 AM UTC
Question

Are STM32 HAL library in compliance to develope with in medicine applications?

Hi, i like to start developing a medicine related product. And i am not quit sure whether to use the STM32 HAL-library or to develope it with the provided LL-library? I am not really expirenced in developing for medicine applications and all it regulations. I have seen some notes on IEC 62304 and misra does HAL library tackle that as well. Can you give me some additional advices or links.

Thanks in advance

This topic has been closed for replies.

2 replies

Tesla DeLorean
Guru
Jan 24, 2022 8:39 AM UTC

No

Expect to take full ownership of responsibility and liability, end-to-end.​

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
Amel NASRI
ST Technical Moderator
Feb 8, 2022 11:29 AM UTC

Hi @Community member​ ,

Some validation reports are available for the STM32Cube HAL & LL drivers. You need to get in contact with your FAE to get them as they are delivered only under NDA.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.