Skip to main content
Associate III
Jun 2, 2025 12:38 PM UTC
Question

Can I use CDC-ECM with H563 ?

Hi, Is ST proved an example of USB CDC-ECM for H563 or something similar I can use for doing a connection between my pc and my nucleo H563 with USB?

This topic has been closed for replies.

5 replies

ST Technical Moderator
Jun 2, 2025 1:09 PM UTC
In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. Saket_Om
Gwen1Author
Associate III
Jun 4, 2025 11:59 AM UTC

Hello @Saket_Om , thanks for your replied.
As I can understand this example works with an SD card for a web server. Did you know if ST provided juste an example of communication between the ST card and PC with CDC-ECM? Like this How to implement the USB Device CDC (VCOM) in STM3... - STMicroelectronics Community but with a board that is similar to H563 ?

ST Technical Moderator
Jun 4, 2025 1:50 PM UTC

Hi @Gwen1 

CDC ACM and CDC ECM are different USB sub classes. Your request is confusing. If you're designing a USB device, the choice between CDC ACM and CDC ECM depends on whether your application requires serial communication or networking capabilities. 

  • CDC ACM is meant for serial communication and is used for devices that need to emulate a COM port over USB like the article you mentioned. 
  • CDC ECM is designed for networking often used to emulate an Ethernet interface over USB.

I hope this helps!

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.Best regards,FBL