Skip to main content
Associate
May 7, 2025 10:18 AM UTC
Question

AN4457 UART Emulation - use via CubeMx?

Split from old (2020), abandoned thread: https://community.st.com/t5/stm32cubemx-mcus/uart-emulation-an4457-is-it-possible-to-use-it-via-cubemx/td-p/310812 for better visibility - and to enable marking a solution...


Hi,

I have the same problem, trying to reverse engineer the AN4457 example for an H7xx MCU using with STM32CubeIDE. Currently my problem is that I need to "#define HAL_UART_EMUL_MODULE_ENABLED " in stm32h7xx_hal_conf.h, but there is not "USER CODE" field, so the define gets overwritten each time I change the IOC file.

I guess the proper approach would be to select the UART_EMUL module in the device configuration tool of the GUI, but I do not know how to make it visible there ...

Did anyone implement this example using an IDE? It would be really helpful for the CubeIDE users.

Thanks!

This topic has been closed for replies.

2 replies

Andrew Neil
Super User
May 7, 2025 10:29 AM UTC

@JR72 wrote:

Currently my problem is that I need to "#define HAL_UART_EMUL_MODULE_ENABLED " in stm32h7xx_hal_conf.h, but there is not "USER CODE" field, so the define gets overwritten each time I change the IOC file.


You could just add it as a Defined Symbol in the Project Properties (Settings) ?

AndrewNeil_0-1746613721577.png

 

PS:

The above is from right-clicking the Project, and choosing 'Properties'.

You can also get to the Define Symbols setting by right-clicking an individual file, or a folder. I've not tried it myself, but I think that should let you apply it to just an individual file, or just a folder ...

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
JR72Author
Associate
May 8, 2025 10:40 AM UTC

Thanks for the workaround, that is a good idea. However, I found that the #define only triggers an #include in the stm32h7xx_hal_conf.h file to activate the module. Since I do not understand how to correctly integrate additional code (i.e. the STSW-STM32156 firmware package) as a module, I decided to give up on this and just implement a user-code solution along the lines of AN4457. A firmware package for the IDE toolchain would nonetheless be great to have.