Skip to main content
Associate II
Nov 24, 2025 6:02 AM UTC
Solved

Using the Nucleo-F411 Board as an ST-LINK Programmer

Hello! I am a student studying STM32.

First of all, thank you very much for your help.

 

First of all, my main concern is that I would like to update the firmware on a board that has the G491RE mounted on it.

However, we do not have an external ST-LINK, and only have a Nucleo-F411 board.

 

Is there any way to use the Nucleo-F411 as an ST-LINK? Or is it possible to obtain the ST-LINK firmware?

Andrew Neil
Andrew NeilBest answer
Super User
Nov 24, 2025 10:40 AM UTC

Although it is possible to use the the ST-Link part of many Nucleo (and some Discovery) boards - as documented in the User Manual - this does have a number of pitfalls; eg, see here.

As I've said here (among others), it can be more trouble than it's worth.

For serious use, I would strongly suggest that you do get a standalone ST-Link - they are not expensive, and are a lot more versatile.

Just be sure to get a genuine one - see here.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.

4 replies

gbm
Super User
Nov 24, 2025 7:35 AM UTC

Most of Nucleo64 boards (the ones with "detachable" top part, including Nucleo-F411) may be used for programming off-board MCUs. Read the Nucleo board's manual; you need to remove two jumpers from "ST-LINK" header and connect at least GND, SWDIO and SWCLK available on the built-in ST-Link "SWD" header to the target MCU (NRST connection may also be useful).

My STM32 stuff on github - compact USB device stack and more: https://github.com/gbm-ii/gbmUSBdevice
mƎALLEm
ST Technical Moderator
Nov 24, 2025 8:42 AM UTC

Hello @ParkPork and welcome to the ST community,

Yes it's possible to use that onboard ST-LINK to connect to an external MCU. You can refer to the user manual of the board: UM1724 STM32 Nucleo-64 boards (MB1136)

Section 7.4 Embedded ST-LINK/V2-1:

mALLEm_0-1763973728906.png

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Andrew NeilBest answer
Super User
Nov 24, 2025 10:40 AM UTC

Although it is possible to use the the ST-Link part of many Nucleo (and some Discovery) boards - as documented in the User Manual - this does have a number of pitfalls; eg, see here.

As I've said here (among others), it can be more trouble than it's worth.

For serious use, I would strongly suggest that you do get a standalone ST-Link - they are not expensive, and are a lot more versatile.

Just be sure to get a genuine one - see here.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
ParkPorkAuthor
Associate II
Nov 27, 2025 8:36 AM UTC

I am deeply grateful for everyone's help.
I will first look into this matter and will provide further updates if necessary.
Thank you.