Skip to main content
Visitor II
Nov 5, 2025 6:06 AM UTC
Question

How to program one NUCLEO-H753ZI Board using another's ST-Link?

Hello ST Community,

I have two NUCLEO-H753ZI boards and I want to use Board 1's on-board ST-Link
to program Board 2's MCU through the CN5 (MIPI-10) connector.

My Setup:
- Board 1 (Programmer): Connected to PC via USB, will provide ST-Link
- Board 2 (Target): Connected via 10-pin ribbon cable to Board 1's CN5
- Both boards are NUCLEO-H753ZI (MB1549 or MB1940)

My Questions:

1. Which jumpers need to be removed on Board 2 to disconnect its on-board
ST-Link from the target MCU?
- I see several connectors with jumpers in the ST-Link section (CN2, JP4, JP5, etc.)
- Which specific jumpers control the SWD connection (SWDIO/SWCLK)?

2. Should jumpers remain installed on Board 1 (the programmer board)?

3. What is the correct CN5 pinout for the MIPI-10 connector on NUCLEO-H753ZI?
- I want to verify my ribbon cable connections are correct

4. For power, should I:
- Power Board 2 through CN5 Pin 3 (VCC) from Board 1?
- Or use separate USB power for Board 2?

5. In STM32CubeIDE, I'm getting "Multiple ST-LINKs detected" error.
How do I configure it to use only Board 1's ST-Link?

What I've Tried:
- Connected both boards via 10-pin ribbon cable on CN5
- Attempted to remove jumpers but unsure which ones are correct
- Getting intermittent connection errors

Any guidance on the correct jumper configuration and connection procedure
would be greatly appreciated!

Thank you!

2 replies

Peter BENSCH
ST Technical Moderator
Nov 5, 2025 8:34 AM UTC

Welcome @Vasanth_L, to the community!

Unfortunately, with the newer NUCLEO-144, the embedded STLINK-V3E can no longer be used to program other targets because the connection between STLINK and the target on that specific NUCLEO-144 cannot be easily disconnected.

You would therefore need to use an ST-LINK that can operate independently: either a separate ST-LINK/V2 or ST-LINK/V3, alternatively one from a NUCLEO-64/-144 with ST-LINK/V2-1, i.e. STM32F103 as the debugger chip, e.g. boards based on MB1137, MB1312 or MB1361 (st.com lists all variants if you are searching for one of these MBxxxx).

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Nov 6, 2025 9:43 AM UTC

To be honest, I'd recommend getting a standalone ST-link: it avoids a lot of faffing around, some pitfalls, and is not expensive.

For example, see this and this.

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.