Skip to main content
Visitor II
Jan 29, 2026 12:41 PM UTC
Solved

Use NUCLEO-N657X0-Q as custom ASIC over Octal SPI?

 Hi,

Can i use the NUCLEO-N657X0-Q board as custom ASIC over an Octal SPI style bus?

Thanks

Atchaiah

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 29, 2026 2:05 PM UTC

@Atch123 wrote:

 Can i use the NUCLEO-N657X0-Q board as custom ASIC over an Octal SPI style bus?


So if I assume I understood your question: that "Nucleo board" will play as a kind of slave of another OSPI master, the answer: that's not possible. OSPI embedded in all STM32 MCUs is always a master and cannot be configured as a slave.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

4 replies

mƎALLEm
ST Technical Moderator
Jan 29, 2026 1:03 PM UTC

Hello @Atch123 and welcome to the ST community,

I don't know if you are colleagues (with this OP post). But that question was almost already asked there ..

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
Jan 29, 2026 1:04 PM UTC

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

 

Your question is unclear: what do you mean by "use the board as a custom ASIC"?

The STM32 is a microcontroller.

 

Does this thread help: STM32N6570-D: Is XSPI/OSPI for memory only, or also external peripherals ?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
Jan 29, 2026 2:05 PM UTC

@Atch123 wrote:

 Can i use the NUCLEO-N657X0-Q board as custom ASIC over an Octal SPI style bus?


So if I assume I understood your question: that "Nucleo board" will play as a kind of slave of another OSPI master, the answer: that's not possible. OSPI embedded in all STM32 MCUs is always a master and cannot be configured as a slave.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
Feb 10, 2026 3:35 PM UTC

Hello @Atch123 ,

Could you please state on this thread please? if your question has been answered please accept the post that has answered your question as solution, otherwise, we (as administrators) we will accept one of the posts listed above as a solution .

Thank you for your understanding.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.