Skip to main content
Associate III
May 20, 2026 7:29 AM UTC
Solved

Two same STM32h757 custom boards: having issue to connect to one board but not the second one

ST moderator: updated the title to be more concise according to the below exchanges.

Hello All,

 

I am facing a problem for debugging one of the board which uses stm32h7 controller.

I am not sure why this is happening but on other board I am able to debug it, but for first one its not working.

Though the code and debug config settings are same for both the board and using same system to debug both, but on one board I am able to debug while on other its is not. so could you please tell me what I can try to resolve this issue.

 

Thanks,

SD 

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
May 20, 2026 12:15 PM UTC

@Shiv09 wrote:

Yes actually both have same schematic, one actually works and other doesnt, but the hint is other board which is not able to debug is getting connected on 1000 freq and just after loading the hex in debug mode its giving below error


It could be a hardware issue.. Solder joint issue..

If you have a third board and it connects, I suggest to return that board to your hardware team to check the PCB.

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

14 replies

Andrew Neil
Super User
May 20, 2026 7:38 AM UTC

You need to give more details - please see: 

How to write your question to maximize your chances to find a solution

 

In particular:

  • Full details of these two boards.
  • Has the non-working board ever worked?
  • What CubeIDE version, on what platform, etc?
  • What debug probe?
  • Does CubeProgrammer work OK?
  • What, exactly, happens when you try to debug? Show error messages, etc ...

 

PS:

See also:

How to solve connection errors when connecting and programming the STM32 target board;

How to solve debugger connection issues

 

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
Shiv09Author
Associate III
May 20, 2026 10:24 AM UTC

Hello @Andrew Neil ,

 

Thanks for the quick reply, The post would be long so hence didn't post lot of details,

here are the details as required.

  • Full details of these two boards.- These are custom board using STM32H757BITb on it
  • Has the non-working board ever worked?- No
  • What CubeIDE version, on what platform, etc?  STM32CubeIDE
    Version: 1.17.0
  • What debug probe? ST Link gdb
  • Does CubeProgrammer work OK?- Yes using the cube programmer I am able to Flash code but have to set frequency to 1800, while other board works on 4000 (able to debug it)
  • What, exactly, happens when you try to debug? Show error messages, etc ... Have attached the images from cubeprogrammer for both frequencies. on 4000 its not getting detected but getting connected at 1800 as in images
  • Shiv09_0-1779271030222.pngShiv09_1-1779271069508.png

     

  •  
  • Shiv09_2-1779271185481.png

     

  • Changed the setting in STM CubeIDE in Debug Config set freq to Auto got above.
  • Changed the frequency to 1000, as here Shiv09_3-1779271534934.png

     

This is what happening after the code is flashed and after few seconds getting "Target is not responding, retrying"

Shiv09_4-1779272749788.png

 

mƎALLEm
ST Technical Moderator
May 20, 2026 10:28 AM UTC

1- Please provide details about the power config of your custom board? LDO? SMPS? what you have configured by software?

2- "I am not sure why this is happening but on other board I am able to debug it, but for first one its not working."

-> Are the boards having the same schematic/hardware?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
May 20, 2026 10:11 AM UTC

Hello,

All STM32H7xx devices are not the same. Their ST boards too.

What board are you using. NUCLEO? DISCO? Custom?

Some boards are configured in SMPS others are in LDO.

So you need to check what power config is set in the board by hardware and set accordingly the power config by software.

But before that you need to recover the board from the power deadlock state: How can I recover my STM32H7/STM32H7RS board after facing a power configuration deadlock?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Shiv09Author
Associate III
May 20, 2026 12:04 PM UTC

Is this helpful or something more is required ?