Skip to main content
Associate
November 12, 2025
Solved

STM32F405RGT6 custom board review

  • November 12, 2025
  • 9 replies
  • 490 views

Hello everyone, this is my first post on the forum. I'm starting to learn STM and have created a custom board using the STM32F405RGT6. This is the first board I've created, and I wanted to check for any errors before sending it to production. So I've uploaded a PDF of the connection diagram. I'd be very grateful if you could review it and let me know if there are any mistakes.

Best answer by mƎALLEm

Hello,

Need to re-check this part of LSE:

mALLEm_0-1763034793828.png

Did you check if the crystal is compatible with the STM32? did you calculate the gain margin based on the crystal characteristics and the load capacitors?

Read How to select a compatible crystal and load capacitors for STM32 with layout guidelines

18pf CL looks a bit high compared to the CL recommended for LSE for STM32 in the AN2867 : 

mALLEm_0-1763035265288.png

9 replies

Andrew Neil
Super User
November 12, 2025

Welcome to the forum.

Please see How to write your question to maximize your chances to find a solution for best results.

 


@ekremtrn wrote:

 I'm starting to learn STM .


Do you have experience with any other microcontroller(s) ?

Before leaping into a custom hardware design, I would strongly recommend that you prototype & gain experience on a development board - far cheaper & easier to find & fix issues than on a custom design!

 

Did you study Application note AN5093, Getting started with STM32G4 Series hardware development boards?

 

I don't see any programming/debug connector ?

Have you considered how you will program, debug & test your design ?

See Design For Debug ...

 

PS:

It would also help to give details on the intended application of this board, and what environment it will operate in - these will affect the design

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
TDK
November 12, 2025

Looks okay except:

How do you plan to program/debug without a programming header?

"If you feel a post has answered your question, please click ""Accept as Solution""."
ekremtrnAuthor
Associate
November 13, 2025

Thank you. I intentionally did not add a programming header because I wanted to design a small card. I plan to program it by removing the RTX and CTX from the 10-pin header and connecting it to the USB-A header with an external cable.

mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
November 13, 2025

Hello,

Need to re-check this part of LSE:

mALLEm_0-1763034793828.png

Did you check if the crystal is compatible with the STM32? did you calculate the gain margin based on the crystal characteristics and the load capacitors?

Read How to select a compatible crystal and load capacitors for STM32 with layout guidelines

18pf CL looks a bit high compared to the CL recommended for LSE for STM32 in the AN2867 : 

mALLEm_0-1763035265288.png

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.