Skip to main content
Brian Khuu
Associate III
October 20, 2019
Question

STM32CubeIDE updated stlink on a stm32H743-EVALv2 board to V3J4M2, but then is unable to program the board.

Was able to program the board previously, but today after updating my STM32CubeIDE, it refused to run debug until I updated the stlink on my dev board.

But upon doing so, it gave these error. Essentially meaning I cannot program my dev board.

```

STMicroelectronics ST-LINK GDB server. Version 5.3.2

Copyright (c) 2019, STMicroelectronics. All rights reserved.

Starting server with the following options:

    Persistent Mode      : Disabled

    Logging Level       : 1

    Listen Port Number     : 61234

    Status Refresh Delay    : 15s

    Verbose Mode        : Disabled

    SWD Debug         : Enabled

Waiting for debugger connection...

Debugger connected

   -------------------------------------------------------------------

            STM32CubeProgrammer v2.2.0          

   -------------------------------------------------------------------

Log output file:  /tmp/STM32CubeProgrammer_TqQf5t.log

ST-LINK SN : 002F001F3137511233333639

ST-LINK FW : V3J4M2

Voltage   : 3.28V

SWD freq  : 24000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Cannot identify the device

Error: unknown or unsupported device (DevID = 0x0000)

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_QKNgwM.srec

 File     : ST-LINK_GDB_server_QKNgwM.srec

 Size     : 157296 Bytes

 Address    : 0x08000000 

Erasing memory corresponding to segment 0:

Download in Progress:

File download complete

Time elapsed during download operation: 00:00:00.199

Verifying ...

Error: Data mismatch found at address 0x08000004 (byte = 0x31 instead of 0x5D)

Error: Download verification failed

Encountered Error when opening /Applications/STM32CubeIDE.app/Contents/Eclipse/plugins/com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.macos64_1.1.0.201910081157/tools/bin/STM32_Programmer_CLI

Error in STM32CubeProgrammer

Debugger connection lost.

Shutting down...

```

I am running this IDE on a mac on MacOS catalina. Oh and btw I still cannot run latest STM32CubeProgrammer on mac, even after updating java to latest version.

This topic has been closed for replies.

29 replies

SFrin
Visitor II
November 15, 2020

Dear Admin, pleas delete my previous post. It belongs to another thread.