Skip to main content
Visitor II
April 3, 2024
Question

STM32 Nucleo F446RE not being detected anywhere on laptop

My STM32 Nucleo F446RE is not being detected on my laptop - neither in my device manager (its not under Ports nor the Universal Serial Bus Controllers dropdowns), nor is it being detected in the Cube IDE. A couple of things I have noticed:
- The power led, LD3, is on when its connected to my laptop, and is red.

- The COM led, LD1, doesn't turn on

- The underside of my board gets hot, even if it's just connected to my laptop, with no other peripherals or devices connected or wired to my STM32 board.
- Note, this isn't my first time flashing code with this specific board. I bought it a month ago and during this month it was working fine, but I was working on a project connected to a motor driver and a power supply, and when I tried to flash the code from the Cube IDE on my board while working on this project, it said "No ST-Link detected! Please connect ST-Link and restart the debug session"
- Also note, I am using ST-Link GDB Server as my debugger if that matters


Troubleshooting solutions I have tried:
- Rebooted my computer

- Rebooted the Cube IDE
- Took the cable out and plugged it back into my computer

- Deleted and reinstalled STM32 Cube IDE and its associated drivers

- Used a different USB-mini cable, and a different port for connecting the board to

Any other possible solutions I can try?

This topic has been closed for replies.

3 replies

Amel NASRI
ST Technical Moderator
May 8, 2024

Hi @asmi-g ,

If you still face the issue, or for any other one who have similar problem, you can find some tips in these 2 articles:

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Tesla DeLorean
Guru
May 8, 2024

>>Any other possible solutions I can try?

Replace?

They shouldn't get hot to the touch unless something is internally shorted.

The boards should not be used on a conductive bench or desk.

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
AScha.3
Super User
May 8, 2024

>The underside of my board gets hot

What about the 2 cpus - hot ?

+

> I was working on a project connected to a motor driver and a power supply

So fried one or both cpus , by a spike or current on gnd / loosing gnd connection, etc.

+

At the price range of this nucleo - replace it (as Tesla said ) and take better care next time, connecting or disconnecting anything with > 5V to a running cpu.

If you feel a post has answered your question, please click on " Best Answer ".