Skip to main content
Moritz1
Associate III
December 11, 2023
Solved

Problkems with NUCLEO-H743ZI2 onboard ST-Link

Hello,
I bought a NUCLEO-H743ZI2 board.

When I plugged it in for the first time, I was able to flash it after two or three attempts (ST-Link was often not recognised).

But now the STM32CubeProgrammer does not recognise the ST-Link at all (I have tried more than 20 times with different USB cables).
When I plug the board into the PC, I get a virtual COM port "STMicroelectronics STLink Virtual COM Port (COM23)" in the device manager.
So the ST-Link seems to communicate. But the programmer still does not recognise it.

What could be the reason?

This topic has been closed for replies.
Moritz1
Moritz1Best answer
Associate III
December 11, 2023

This is not my Problem.

My problem was that the on-board ST-Link was not recognices.

But I found a solution: This problem only happens if I connect the NUCLEO Board via my USB hub to the Laptop.

If I connect it directly to the Laptop it works fine.

3 replies

Mike_ST
ST Technical Moderator
December 11, 2023

Hello,

Please have a look at this post:

Unable to connect to STM32H7 devices 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
Moritz1
Moritz1AuthorBest answer
Associate III
December 11, 2023

This is not my Problem.

My problem was that the on-board ST-Link was not recognices.

But I found a solution: This problem only happens if I connect the NUCLEO Board via my USB hub to the Laptop.

If I connect it directly to the Laptop it works fine.

Tesla DeLorean
Guru
December 11, 2023

Hubs and Docking Stations have historically been an issue. Gets particularly troublesome with External Loaders, and pushing 8 - 32MB of data, and the connection randomly failing mid process. Issue with board/drivers and ability to recover / retry

Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..