Skip to main content
RNiel.2
Associate II
January 9, 2025
Question

Inconsistent behaviour on NUCLEO-H755ZI-Q

Hi,

I am currently working on a project using the NUCLEO-H755ZI-Q development board.

I am testing with a simple program that turns on the green led and goes to a while loop. I start with "full chip erase" then flash my testing program to the M7 core. I have an issue with one of my nucleo boards where it sometimes get stuck(?) during startup. When I press the reset button on the board it's 50/50 if it will boot up correctly and light up the green LED, or go into a stuck state where I can't reprogram it.

I have a second identical board to test with that doesn't have this issue. I have tried in CubeProgrammer to export all the settings from the "good" board and import them to the "bad" board, but it didn't change the behaviour.
I have also looke at the "-ob displ" output and only the serial number was different.

Any ideas of what to try next?

This topic has been closed for replies.

1 reply

Mike_ST
ST Technical Moderator
January 9, 2025

Hello,

Please check that BOOT0 pin is not floating and set to 0V.

Check these articles for common problems with STM32H7:

How to unbrick an STM32H7 after setting the wrong power mode 

Unable to connect to STM32H7 devices 

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.