Skip to main content
Associate
June 3, 2024
Question

"Error in initializing ST-LINK device. Reason: No device found on target." STM32H743IIT6

I desinged a custom board using STM32H743IIT6. But I can't Debug it.

  • Reset is pulled high
  • Boot0 is pulled low
  • VDD is stable at 3..28V at all desired pins of the board
  • VCAP 1&2 connected to 2.2uF capacitors...
  • VDDA is 3.28V, VSSA is Grounded

    I tried manything but I couldn't debug it. Using ST-LinkV2.
This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
June 25, 2024

Hi @_CEVVAL ,

Some recommendations:

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.