Skip to main content
Associate II
August 28, 2024
Solved

Connecting issue Nucleo-H7A3ZI - Q

Hello I can't able to connect my NUCLEO - H7A3ZI -Q. Its showing error while commenting.

Durgasish_0-1724824641884.png

Please help me with solving this issue.

This topic has been closed for replies.
mƎALLEm
mƎALLEmBest answer
ST Technical Moderator
August 29, 2024

Visually, I don't see issue on the board according to the images you shared.

For Solution 1, please check again by following this article:

https://community.st.com/t5/stm32-mcus/how-to-unbrick-an-stm32h7-after-setting-the-wrong-power-mode/ta-p/49691

BOOT_CM7_ADD1 is not accessible as it's located in option bytes and you couldn't connect to the board with STM32CubeProgrammer to check.

 

 

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.

20 replies

STTwo-32
ST Technical Moderator
August 28, 2024

Hello @Durgasish and welcome to the ST Community :smiling_face_with_smiling_eyes:.

the STM32 ST-LINK utility is now obsolete. Could you please try using STM32CubeProgrammer. Also, don't forget to use a data and not a charging cable.

Best Regards.

STTwo-32

 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
DurgasishAuthor
Associate II
August 28, 2024

Hello @STTwo-32  if I'm using in STM32Cube IDE also I'm getting similar issue.

Stmh7A3_issue.png

STTwo-32
ST Technical Moderator
August 28, 2024

Could you try to perform a mass erase of the board using CubeProgrammer. Then, restart CubeIDE and retry to connect. 

Also, make sure that your ST-Link firmware is upgraded, check the jumpers, SWD pins status, try configuring the "Connect under reset" mode and dont forget to check your power supply and try to change your USB cable (ensure that you are using a data cable not a charging one).

Best Regards

STTwo-32

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
mƎALLEm
ST Technical Moderator
August 28, 2024

Are you sure the board has not used or/and modified by someone else ? Do you have another board and connect with STM32CubeProgrammer?

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
DurgasishAuthor
Associate II
August 28, 2024

No It is not modified by anyone. And yes I have checked it with another NUCLEO H743ZI its working fine for that board.

Andrew Neil
Super User
August 28, 2024

@Durgasish wrote:
AndrewNeil_1-1724837505880.png

So did you do that?

Also:

AndrewNeil_2-1724837554027.png

Does that apply to you situation? If so, did you do it?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
DurgasishAuthor
Associate II
August 29, 2024

Yes I did that way.

 

Mike_ST
ST Technical Moderator
August 29, 2024

Hello,

just in case, please have a look to that article:

Unable to connect to STM32H7 devices  

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question. 
DurgasishAuthor
Associate II
August 29, 2024

Thankyou very much each of you for all the supports. I recovered my board and now my board is working fine.