Skip to main content
Associate III
Feb 15, 2025 5:25 PM UTC
Solved

Cannot connect to B-U585I-IOT02A Discovery kit for IoT node with STM32U5 series

All of a sudden,  I cannot connect to this board via stlink usb cable.  I tried pressing reset button, updated firmware, connect in every possible mode (hardware reset, core reset).  Is there a combination/sequence of pressing buttons? In other stm32 mcu I saw  a way to erase memory by connecting a resistor to reset pin and  ground momentarily.  Can this be done on this board and how?   Anything else i can try before I trash it?   Thank you for your help!

 

This topic has been closed for replies.
psabelaBest answer
Associate III
Apr 7, 2025 2:16 AM UTC

OMG!  I must have accidentally slid off the little plastic jumper connector connecting JP4 off of the pins.  (Not an electrical guru here.)  I only noticed it when comparing to an identical board that I subsequently purchased thinking I must have damaged this one.   Anyhow, the plastic connectors that slide onto both JP4 or JP3 are important -- I was not able to established connection to the board without either one.

2 replies

KDJEM.1
ST Technical Moderator
Feb 25, 2025 2:41 PM UTC

Hello @psabela,

 

Could you try with another USB cable? Which error did you get?

I recommend you to look at these FAQs: 

These articles describe tips to prevent or fix errors encountered when connecting the STM32 target board to your computer.

 

I hope this will help you to solve the issue.

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
psabelaAuthorBest answer
Associate III
Apr 7, 2025 2:16 AM UTC

OMG!  I must have accidentally slid off the little plastic jumper connector connecting JP4 off of the pins.  (Not an electrical guru here.)  I only noticed it when comparing to an identical board that I subsequently purchased thinking I must have damaged this one.   Anyhow, the plastic connectors that slide onto both JP4 or JP3 are important -- I was not able to established connection to the board without either one.