Skip to main content
gcrisa
Associate II
August 17, 2020
Solved

[BUG] ST-Link firmware verification - No ST-LINK detected message since 1.4.x update.

  • August 17, 2020
  • 64 replies
  • 18226 views

On Windows 10, I just updated (again) to the 1.4.2 version, hoping to solve this issue, yet nothing changed.

Already tried a clean install (again) and re-installed the latest STM32CubeProgrammer: nothing changed.

Will ST handle this sooner or later please? Or at least give some help in diagnosing the problem? Thanks

This topic has been closed for replies.
Best answer by LaurentL

Yes of course, it will be included for next releases.

Edit after it was marked as best answer :

The libusb dll v1.0.23 is now installed with STM32cubeIde v1.5.0 installer.

So, no need to patch it, just install (not update) STM32CubeIde v1.5.0.

Rgds,

Laurent

64 replies

gcrisa
gcrisaAuthor
Associate II
August 17, 2020

Forgot to add:

  • have the exact same issue on a different PC running Windows 10 (latest build)
  • already updated the ST-Link firmware on all the boards i tested
  • installed the ST-Link Utility too: both the Utility and CubeProgrammer can connect to the target without any issues
  • nothing is displayed in any of the console/output windows in the CubeIDE so I can't even know what is happening
  • the J-Link programmer is running fine
EJOHA
Associate
August 18, 2020

It sounds that there is some problem with the installation but you have already tried clean installation. Did you download the installer again, before re-installation?

Could you please try some of these ways to identify the reason of this problem.

Try to use OpenOCD

Instead of ST-LINK GDB server try to use OpenOCD. Open the Debug Configuration and change to gdb server to OpenOCD. Does it work to debug with OpenOCD in STM32CubeIDE?

ST-LINK GDB server

Try to run ST-LINK GDB server manually from console view. Open File explorer and search for ST-LINK_gdbserver.exe in STM32CubeIDE installation. Open this folder and change directory in console view to this one. E.g. C:\ST\STM32CubeIDE_1.4.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_1.4.0.202007081208\tools\bin

Then search for STM32_Programmer_CLI.exe in STM32CubeIDE installation (start search from root of STM32CubeIDE installation). Open this folder. E.g. C:\ST\STM32CubeIDE_1.4.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.4.0.202007081208\tools\bin

In console view start ST-LINK GDB server with parameters -d (swd mode) and -cp (folder location to CubeProgrammer) E.g.

C:\ST\STM32CubeIDE_1.4.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_1.4.0.202007081208\tools\bin>ST-LINK_gdbserver.exe -d -f mylog.txt -cp C:\ST\STM32CubeIDE_1.4.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.4.0.202007081208\tools\bin

What does it log in console or into log file ?

More info about ST-LINK GDB server and how to connect to use it is found from STM32CubeIDE "Information Center". The STM32CubeIDE User manual also contains detailed info. This User manual is not yet included in documentation listed in Information Center but can be found here:

https://www.st.com/resource/en/user_manual/dm00629856-description-of-the-integrated-development-environment-for-stm32-products-stmicroelectronics.pdf

gcrisa
gcrisaAuthor
Associate II
August 18, 2020

Hello, thank you so much for your answer.

Yes, each re-installation attempt was made with the most recent installer available on the website.

Selecting OpenOCD changes nothing actually, the exact same error pops up immediately as soon as I try to start a debug session.

I just tried to start the ST-LINK GDB server manually from the console, following your instructions and the server seems to start actually! I attached the log file.

By the way, all the folder names on my setup are identical to the ones you posted, so I'm guessing my tools versions are correct right?

Having the ST-LINK GDB server started in the console, I tryed to change the debug configuration to "Connect to remote GDB server" instead of "Autostart local GDB server" and it worked (both selecting ST-LINK GDB and ST-LINK OpenOCD), so it seems the IDE can't start the server for some reason... Any clue how can I discover why?

Thanks again so far, your help is much appreciated.

LaurentL
ST Employee
August 18, 2020

Hello,

Can you check that the stlink server exe is installed properly and running in task manager ?

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
gcrisa
gcrisaAuthor
Associate II
August 18, 2020

Sure but how? I thought the server is actually started when I start a debug session from the IDE?!

EJOHA
Associate
August 18, 2020

The STLink Server is a utility which should be started by STM32CubeIDE when a debug session is started. It is not the same program as the ST-LINK GDB server. The STLink Server makes it possible for several applications to connect in parallel to an ST-LINK. The "STLink Server for STLink devices" is when it is running listed in Windows Task Manager - Users tab.

When ST-LINK GDB server is started manually you can add the -t option to let STLink Server to start.

Please try this and observ in Task manager if server is started and running.

gcrisa
gcrisaAuthor
Associate II
August 18, 2020

Got it.

Well, for sure the IDE does not start it, because the debug session doesn't start at all (that error shows immediately when I click the debug button).

I tried adding the -t option to the command line but with that the ST-LINK GDB server refuses to start, and of course no STLink Server in the Task Manage (see the attached log).

gcrisa
gcrisaAuthor
Associate II
August 18, 2020

I just checked from the Windows Control Panel: "STMicroelectronics stlink-server" is installed, version 1.3.0-4.

EJOHA
Associate
August 18, 2020

Do you have ST-LINK connected directly to USB port on PC or via a hub?

If a hub is used try to connect ST-LINK / board directly to PC.

gcrisa
gcrisaAuthor
Associate II
August 18, 2020

All of my attempts have been done with the boards connected to the PC(s). I tried:

  • NUCLEO-F401RE fw. revision V2.J37.M26
  • STLINK-V3MINI fw. revision V3.J7.M2

LaurentL
ST Employee
August 18, 2020

Did you try with other USB port and connect only one board at a time.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
ilyaz yilmaz
Associate II
August 24, 2020

Actually I Updated to 1.4.2 and I faced the same problem. I removed all files and all programs.

I installed from STM32Cubeide from zero but it didnt work. I m waiting a solution???

PJ SA.1
Visitor II
August 26, 2020

i have the same problem too, 1.4.x work perfectly on my new HP laptop, but not working on my old DELL laptop. no st-link detected when star debug. is the problem solved ?

PJ SA.1
Visitor II
August 26, 2020

this are my temporary solution

  1. at the moment for make ver 1.4.x debug work, i siwtch debug configguration to remote gdbserver option0693W000002lA4oQAE.jpg
  2. modify config.txt in the folder "C:\ST\STM32CubeIDE_1.4.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.stlink-gdb-server.win32_1.4.0.202007081208\tools\bin" for correct path   for STM32_Programmer_CLI executable0693W000002lA61QAE.jpg
  3. Start ST-LINK_gdbserver.bat manually, it will launch win cmd prompt0693W000002lA6VQAU.jpg
  4. start debugging from stmcubeide and it's work0693W000002lA74QAE.jpg0693W000002lA6kQAE.jpg

gcrisa
gcrisaAuthor
Associate II
August 26, 2020

Hi, sad to hear I'm not the only one facing this issue. If you can, please take some time to do the tests that LaurentL asked me to do, so we can know if it's actually the same issue, and they can eventually fix it: in my case it seems that the libusb (used by the stlinkserver.exe) is not able to enumerate the USB devices...

PJ SA.1
Visitor II
August 26, 2020

hi It also works on my old dell laptop.

awesome, That is great, many thanks!!0693W000002lLxuQAE.jpg