Skip to main content
Associate III
August 23, 2024
Question

BOARD STM32 NUCLEO-F334R8

i am using nucleo-f334r8 and when i connect to the laptop the MCU is hot but the voltage on the VDD does not exceed 3.36V. I want to use another MCU therefore I want to use the DEBUGGER (top part) also what should I unplug (jamper) or should I connect?

board nucleo.jpg

 

This topic has been closed for replies.

3 replies

STTwo-32
ST Technical Moderator
August 23, 2024

Hello @macam1 

I think this post should be helpful for you. On your case, CN2 connecter should be off.

Screenshot_2024-08-23-08-57-12-64_e2d5b3f32b79de1d45acd1fad96fbb0f.jpg

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
macam1Author
Associate III
August 23, 2024

yes, I have done that, but the MCU is still hot, I want to use another MCU outside of the built-in MCU but I need to disconnect the connection between the debugger and the built-in MCU. I have removed the jumper on the ST_link. I wonder if there are still other jumpers that need to be removed?

STTwo-32
ST Technical Moderator
August 23, 2024

Everything you need to do is mentionned on the part 6.2.4 of the UM1724.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.