Skip to main content
Associate III
September 20, 2025
Question

32F469IDISCOVERY - pre-installed demo not showing on LCD

hello all,

i bought multiple 5 unit of 32F469IDISCOVERY and tested them all not a single one lcd shows pre installed demo. so i bought 2 more uniits from different vender but foud same issue. what would be the possible cause? ia some one got same issue?

3 replies

mƎALLEm
ST Technical Moderator
September 20, 2025

Hello,

The issue is not clear. Please decribe the issue in more details..

Is it linked to this thread (I didn't accept the solution in it)?

 

To give better visibility on the answered topics, please click "Best answer" on the reply which solved your issue or answered your question.
Andrew Neil
Super User
September 24, 2025

Where did you buy them?

have you taken this up with the seller?

A complex system that works is invariably found to have evolved from a simple system that worked.A complex system designed from scratch never works and cannot be patched up to make it work.
EXUE.2
ST Employee
October 27, 2025

yes, you are right, for the STM32F469_DK board production from year 2022, we didn't keep demo in the Flash, so you can't see the demo and display on LCD. but you can download the examples from STM32 official Cube to test it.