Skip to main content
B.Montanari
ST Technical Moderator
Mar 19, 2026 3:30 PM UTC

How to use the MCO with STM32CubeMX2

Summary

This article provides a step-by-step guide to configuring and verifying the master clock output (MCO) on an STM32 microcontroller. The workflow includes initial hardware configuration in STM32CubeMX2, project management using CMake, and project initialization and execution in Visual Studio Code. By the end of this guide, you have a functional project that outputs a 1 MHz clock signal from the microcontroller’s PA8 pin.

Introduction

In embedded systems development, outputting internal clock signals to external pins is essential for debugging, synchronization, and driving peripheral components. The master clock output (MCO) feature in STM32 microcontrollers enables engineers to monitor internal oscillators or the system clock on a physical pin.

This guide describes the register settings and clock tree configurations required to generate a 1 MHz signal. It provides a clear path for developers to configure STM32 hardware in a professional Visual Studio Code environment.

Prerequisites

Install the following tools:

The hardware used in this tutorial is the NUCLEO-C562RE board.

1. STM32CubeMX2 project creation and basic setup

Follow these steps to create the MCO application project for the NUCLEO-C562RE board:

Open STM32CubeMX2. On the Home page, click the MCU square to create a new project.

BMontanari_0-1769541272670.pngIn the search field under MCU name, enter STM32C562RE and select your board. Click Continue.

BMontanari_1-1769541272673.png

Enter your project name and location. Click [Automatically Download, Install & Create Project] to finish project creation.

BMontanari_2-1769541272676.png

Click [Launch Project] to get started.

BMontanari_3-1769541272678.png

1.1 Pinout and peripheral configuration

After the project workspace is ready, locate pin PA8 in the Pinout view. Right-click the pin and select RCC_MCO1 to assign it as the master clock output pin.

BMontanari_4-1769541272691.png

In the left Categories menu, navigate to System Core and select the RCC peripheral to open its configuration panel. In the RCC configuration settings, enable the MCO1 (master clock output 1) feature.

BMontanari_5-1769541272699.png

In case you failed to allocate it at PA8, you can use the System portion to specify which pin you want the MCO1 to be placed at.

BMontanari_6-1769541272699.png

1.2 Clock configuration

Switch to the Clock Configuration tab.

BMontanari_7-1769541272708.png

Adjust it in accordance with the desired clock branch that your application wants to evaluate. In this case, the selected output was adjusted for 2 MHz, coming from the PSIK:

BMontanari_8-1769541272708.png

 BMontanari_9-1769541272710.png

To achieve a 1 MHz output clock, locate the MCO1 Mux. Select the desired source and set the MCO1 prescaler (divider) to 8.

BMontanari_10-1769541272711.png

1.3 Code generation

To generate the code:

  1. Click on the [Project settings] icon and select the desired IDE.
  2. Click the [Generate] button.

BMontanari_11-1769541272714.png

2. Configuring the project in Visual Studio Code

Open Visual Studio Code and open the project folder.

You are prompted with a selection. In case you miss click or that does not appear, press Ctrl+Shift+P, type CMake: Select Configure Preset, and choose your debug configuration.

BMontanari_12-1769541272715.png

Build the project to ensure that everything is properly set and then go to the implementation code.

BMontanari_14-1769541272718.png

2.1 Validation

After building the application, locate the [Run and Debug] icon, create your debug session by selecting the STLINK GDB Server option:

BMontanari_15-1769541272719.png

BMontanari_16-1769541272719.png

Connect the oscilloscope to PA8 and GND to verify the clock output.

BMontanari_17-1769541272722.png

Scope/Data trace image:

BMontanari_18-1769541272723.png

Conclusion

By following these steps, you have successfully configured and deployed your project. In this guide, we focused on enabling and verifying the Master Clock Output (MCO) using the STM32CubeMX2 configuration.

Related links