FAQ: STM32H7 - How to read RAMECC_MxFAR failing address
- 13 replies
- 8306 views
- How to access to the right RAMECC monitor to get the RAM failing address when an ECC error occurs?
- How to translate the content of the failing address register to the actual RAM address (e.g. FADD= 0x2004)?
Note: For simplicity and clarity, the description is based on the STM32H74x/5x series. The description would be similar for other STM32H7 series and can be found in the reference manual.
1. RAMECC controllers
The number of controllers depends on the STM32H7 series.
- The STM32H74x/5x and STM32H72x/3x has one RAMECC controller per power domain.
-
RAMECC controller for Domain 1 (D1) = RAMECC1
-
RAMECC controller for Domain 2 (D2) = RAMECC2
-
RAMECC controller for Domain 3 (D3) = RAMECC3
-
- The STM32H7Ax/Bx has only one RAMECC controller.
-
RAMECC controller for the CPU Domain (CD) = RAMECC
-
2. RAMECC monitors
The list of monitors varies depending on the STM32H7 series.
The STM32H74x/5x has one monitor for each RAM block in the MCU.
- RAMECC1 controller has 5 monitors for D1
- RAMECC2 controller has 5 monitors for D2
- RAMECC3 controller has 2 monitors for D3
The detail is given in table 11 of the reference manual.
3. RAMECC registers address
From table 8 of the reference manual:
| Boundary address | Peripheral |
|---|---|
| 0x58027000 - 0x580273FF | RAMECC3 |
| 0x52009000 - 0x520093FF | RAMECC1 |
| 0x48023000 - 0x480233FF | RAMECC2 |
4. RAMECC exception vectors
From table 143 of the reference manual:
| Signal | Priority | NVIC position |
Acronym | Description | Address offset |
|---|---|---|---|---|---|
| ramecc1_it | 152 | 145 | RAMECC1 | ECC diagnostic global interrupt for RAMECC D1 | 0x0000 0284 |
| ramecc2_it | RAMECC2 | ECC diagnostic global interrupt for RAMECC D2 | |||
| ramecc3_it | RAMECC3 | ECC diagnostic global interrupt for RAMECC D3 |
5. RAMECC registers - e.g. RAMECC1
For RAMECC1, the boundary addresses are 0x52009000 - 0x520093FF (table 8 of the reference manual).
The addresses of the registers for each monitor are as follows:
- RAMECC_IER -- interrupt enable
=> 0x52009000
- RAMECC_MxCR -- configuration
=> 0x52009000 + 0x20 * x with x = [1..5]
- RAMECC_MxSR -- status
=> 0x52009044 Monitor 2
=> 0x52009064 Monitor 3
=> 0x52009084 Monitor 4
=> 0x520090a4 Monitor 5
- RAMECC_MxFAR -- failing address
=> 0x52009068 Monitor 3
=> 0x52009088 Monitor 4
=> 0x520090a8 Monitor 5
- RAMECC_MxFDRL -- failing data low
=> 0x5200904c Monitor 2
=> 0x5200906c Monitor 3
=> 0x5200908c Monitor 4
=> 0x520090ac Monitor 5
- RAMECC_MxFDRH -- failing data high
=> 0x52009030 + 0x20 * (x-1) with x = [1..5]
=> 0x52009030 Monitor 1
=> 0x52009050 Monitor 2
=> 0x52009070 Monitor 3
=> 0x52009090 Monitor 4
=> 0x520090b0 Monitor 5
- RAMECC_MxFECR -- failing ECC error code
=> 0x52009034 + 0x20 * (x-1) with x = [1..5]
=> 0x52009034 Monitor 1
=> 0x52009054 Monitor 2
=> 0x52009074 Monitor 3
=> 0x52009094 Monitor 4
=> 0x520090b4 Monitor 5
6. How to get the failing address from the content of RAMECC_MxFAR
The information given by the RAMECC_MxFAR register is described in the reference manual as the failing address (FADD) for the monitor x.
In fact, the address in FADD[31:0] is relative and it points to a word, not a bit. To calculate the actual RAM address, the following formula must be applied:
Example with FADD= 0x2004:
|
0x2400 0000 + 0x2004 * 8 = 0x2401 0020 |
|
0x3000 0000 + 0x2004 * 4 = 0x3000 8010 |
7. Related links
RAM ECC monitoring is described in the reference manual - section 3 - RAM ECC monitoring (RAMECC).
-
RM0433 STM32H742, STM32H743/753 and STM32H750 Value line advanced Arm®-based 32-bit MCUs
-
RM0468 STM32H723/733, STM32H725/735 and STM32H730 Value line advanced Arm®-based 32-bit MCUs
-
RM0455 STM32H7A3/7B3 and STM32H7B0 Value line advanced Arm®-based 32-bit MCUs
The error correction code (ECC) management and implementation on STM32 microcontrollers is described in:
-
AN5342 How to use error correction code (ECC) management for internal memories protection on STM32 MCUs
This article was originally published 2022-06-02.
Before republication the article had 271 views.