Skip to main content
Christophe VRIGNAUD
ST Employee
Oct 22, 2024 1:00 PM UTC

FAQ: Fixing STM32 FDCAN communication disruptions - APB bus, kernel, and time quanta clocks

  • Aug 7, 2026 4:01 PM UTC
  • 1 reply
  • 2437 views

Introduction 

This article dives into how you can avoid communication disruptions. In some cases, you may see that FDCAN messages are repeated even though they’re acknowledged. You may also observe some other unexpected behavior. We cover a possible cause of the issue and how to solve it. 

1. Complying with the relation between the clocks 

When a communication issue appears, a possible cause can be the noncompliance to the following rule shown below.

The FDCAN requires that the CAN time quanta clock is always below or equal to the APB clock.

 

 

fdcan_tq_ck   ≤   fdcan_pclk

 

 

 

2. Clocks applied to the FDCAN peripheral

Two clocks are applied to the FDCAN peripheral as shown on the following table extract from the reference manual of STM32H5 (RM0481).

 

2024-10-11 16_32_14-STM32H523_33xx, STM32H562_63xx, and STM32H573xx Arm_Sup_®__Sup_-based 32-bit MCU.png

 

The kernel clock directs to the FDCAN core, which manages the CAN protocol, the communication lines, and the baud rate.

The APB clock allows configuration and control of the FDCAN subsystem through registers, and also to access the message RAM.

 

3. FDCAN subsystem block diagram

 

STM32N6, STM32H7
(except STM32H7RS)

STM32L5, STM32U3, STM32U5, STM32C092, STM32G0, STM32G4, STM32H5, STM32H7RS

2024-10-14 13_44_14-STM32H723_733, STM32H725_735 and STM32H730 Value line advanced Arm®-based 32-bit.png 2024-10-14 13_45_02-STM32G4 series advanced Arm_Sup_®__Sup_-based 32-bit MCUs - Reference manual and.png

The two block diagrams above are extracts respectively of the reference manual of STM32H72x/3x (RM0468) and of the reference manual of the STM32G4 (RM0440).

They display both 3 FDCAN units and a common block on the top. The clock domains, APB and kernel, are displayed with different colors: light and dark gray, or light yellow and gray.

The FDCAN peripheral is connected to the APB1 peripheral bus (refer to the MCU block diagram in the datasheet, generally figure 1). In STM32CubeMX, the FDCAN peripheral clock fdcan_pclk is the APB1 peripheral bus clock as shown in the image below.

 

2024-10-11 14_23_32-Clipboard_modified.png

 

The kernel clock fdcan_ker_ck is delivered through a multiplexer allowing to choose among several sources.

 

2024-10-11 15_02_00-STM32CubeMX Untitled__ STM32H725ZGTx.png

 

4. FDCAN time quanta clock

The FDCAN cores are clocked by a common FDCAN time quanta clock fdcan_tq_ck that is used to define the baud rate of the communication channel.

As shown on the block diagram, this clock is generated from the kernel clock as follows:
 

fdcan_tq-ck   =   fdcan_ker_ck / DIV
 

Depending on the STM32 series, the divider is defined by the CDIV[0..3] bits in the FDCAN_CCU_CCFG register (STM32H7) or by the PDIV[0..3] bits in the FDCAN_CKDIV register (for other STM32 series).

The value by default is DIV = 1. When necessary, the divider can be modified to comply with the rule given above between the time quanta clock and the APB clock (fdcan_tq_ck ≤ fdcan_pclk).

The table below summarizes the conditions applying to DIV.

 

 

STM32N6, STM32H7
(except STM32H7RS)

STM32L5, STM32U3, STM32U5, STM32C092, STM32G0, STM32G4, STM32H5, STM32H7RS

2024-10-14 13_44_14-STM32H723_733, STM32H725_735 and STM32H730 Value line advanced Arm®-based 32-bit.png 2024-10-14 13_45_02-STM32G4 series advanced Arm_Sup_®__Sup_-based 32-bit MCUs - Reference manual and.png

 

 

DIV in [1..30]

DIV in [1..30]

-------

The CCU (clock calibration unit) is common

to all FDCAN units.

-------

Only FDCAN1

has access to CCU registers.

-------

IF CCU is bypassed

 

The DIV is set at initialization by the application to fulfill the CAN time quanta clock requirement.

-------

IF CCU is enabled

The DIV is managed by the CCU
 

Baud rate prescalers
Prescaler = 0
(nominal and data prescalers for all the FDCAN units)

Kernel clock
fdcan_ker_ck > 80 MHz
 

FDCAN bitrates
 Nominal bitrate < 1 Mbit/s
 Nominal bitrate < data bitrate < 8 Mbit/s

-------

The configuration is common

to all FDCAN units.

-------

Only FDCAN1

has access to the CKDIV register.

-------

 


The DIV is set at initialization by the application to fulfill
the CAN time quanta clock requirement.

 

Conclusion

The FDCAN requires that the CAN time quanta clock is always below or equal to the APB clock.

 

 

fdcan_tq_ck   ≤   fdcan_pclk

 

 

 

When necessary, a divider is applied between the kernel clock and the time quanta clock to comply with this rule.

fdcan_tq-ck   =   fdcan_ker_ck / DIV

Related links

 

1 reply

Bowman32
ST Employee
Jun 23, 2026 1:59 PM UTC

Hi,

The FDCAN specification has been updated. The FDCAN requires that the CAN time quanta clock is always below or equal to the APB clock (fdcan_tq_ck ≤ fdcan_pclk).

For reference you could refer to RM0517 Rev 1 section Bit timing.