Skip to main content
RShiv.1
Associate III
Mar 2, 2021 7:32 AM UTC
Solved

SPI interface for STM32L476VG

STM32L476VG is the MCU we are interfacing with ST25R3911B using SPI.

what we have understood from some search is that we need RFAL (abstraction layer) to interface with RF HAL.

Then once we integrate RFAL and RF HAL in our system workbench(ac6) project we need to build the integration then use SPI calls to read the register from RFID reader ST25R3911B

we wanted to use ISO-14443A standard to be configured and read the values.

where do we get the basic RFAL work space or code flow so that we shall use in our current project?

Kindly guide us and let us know are we in right path?

This topic has been closed for replies.
Brian TIDAL
Brian TIDALBest answer
ST Technical Moderator
Mar 2, 2021 8:28 AM UTC

Hi,

X-CUBE-NFC5 package provides an NFC polling demo using the RFAL and running on NUCLEO-L476RG (MCU board) + X-NUCLEO-NFC05A1 (ST25R3911B expansion board). It can be a good starting point for a project based on SYM32L476VG.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

190 replies

RShiv.1
RShiv.1Author
Associate III
May 20, 2021 11:30 AM UTC

Hi BT,

As you told we probed the Interrupt line in ST25R3911B  to STM32L476VG and we are seeing no activity here...any guess on what could be the problem and how we can

solve this?..kindly let us know.

regards

Ravi

Brian TIDAL
ST Technical Moderator
May 20, 2021 11:37 AM UTC

Hi,

the interrupt line is probably still connected to the onboard ST25R3911B and conflicting with the off board ST25R3911B ...

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RShiv.1
RShiv.1Author
Associate III
May 20, 2021 11:48 AM UTC

Hi BT,

we are using X-NUCLEO-NFC05A1 connected discovery board STM32L476VG(not our customized board)...so where is the conflict here..also ensured no other lines are

connected ...any directions here..

regards

Ravi

RShiv.1
RShiv.1Author
Associate III
May 20, 2021 11:53 AM UTC

Hi BT,

is it a S/w issue or Hardware...if its hardware..then where could be the issue..

regards

Ravi

RShiv.1
RShiv.1Author
Associate III
May 20, 2021 11:59 AM UTC

Hi BT,

ALL SPI lines we are seeing CLK,MISO and MOSI properly no issues with that.

Brian TIDAL
ST Technical Moderator
May 20, 2021 12:11 PM UTC

HI,

if the SPI is working properly, if you see proper responses from ST25R3911B on MISO, well, I would say it looks like either an HW issue (line being pulled up by another device) or the MCU GPIO is not properly configured (i.e. GPIO being in output pull up mode). Please provide a logic analyzer trace so I can check SPI communication is correct.

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RShiv.1
RShiv.1Author
Associate III
May 20, 2021 12:14 PM UTC

Hi BT,

Fine we will check this..but we do not have an analyser trace..we will share you the trace from scope(oscilloscope)..should be fine right.

regards

Ravi

Brian TIDAL
ST Technical Moderator
May 20, 2021 12:22 PM UTC

Hi,

1/ can you confirm you see the following log message:

  • "Initialization succeeded..\r\n"
  • "SPI init passed..\r\n"?

2/ disconnect the interrupt line from the ST25R3911B and connect the GPIO on 3V3 and then on Gnd: do you see the interrupt being triggered on MCU side?

Rgds

BT

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
RShiv.1
RShiv.1Author
Associate III
May 20, 2021 12:27 PM UTC

Hi BT,

we are getting SPI

  • yes we are getting Initialization succeeded..\r\n"
  • "SPI init passed..\r\n"?

we will answer the 2nd one for you shortly.

regards

Ravi

RShiv.1
RShiv.1Author
Associate III
May 20, 2021 1:46 PM UTC

Hi BT,

we did the test for the 2nd point and still not seeing any result..I have also attached the ioc.file..can you confirm whether we need to configure PA3 as GPIO_EXTI3 or as GPIO_INPUT...let me know whether the configurations are correct..

regards

Ravi