Skip to main content
GerHebert
Associate II
March 21, 2022
Question

ADC do not work with 1.10 after migration.

The clock "to ADC (MHz)" is grey in clock configuration. Don't see prescaler field in configuration. Plus it remove PLL **** configuration in main.c.

 /* Configure the system clock */
 SystemClock_Config();
 
//****** This below have been remove from my last commit! *********
/* Configure the peripherals common clocks */
 PeriphCommonClock_Config();
// ******
 
//****** And this:
/**
 * @brief Peripherals Common Clock Configuration
 * @retval None
 */
void PeriphCommonClock_Config(void)
{
 RCC_PeriphCLKInitTypeDef PeriphClkInitStruct = {0};
 
 /** Initializes the peripherals clock
 */
 PeriphClkInitStruct.PeriphClockSelection = RCC_PERIPHCLK_ADC;
 PeriphClkInitStruct.PLL2.PLL2M = 4;
 PeriphClkInitStruct.PLL2.PLL2N = 9;
 PeriphClkInitStruct.PLL2.PLL2P = 2;
 PeriphClkInitStruct.PLL2.PLL2Q = 2;
 PeriphClkInitStruct.PLL2.PLL2R = 2;
 PeriphClkInitStruct.PLL2.PLL2RGE = RCC_PLL2VCIRANGE_3;
 PeriphClkInitStruct.PLL2.PLL2VCOSEL = RCC_PLL2VCOMEDIUM;
 PeriphClkInitStruct.PLL2.PLL2FRACN = 3072;
 PeriphClkInitStruct.AdcClockSelection = RCC_ADCCLKSOURCE_PLL2;
 if (HAL_RCCEx_PeriphCLKConfig(&PeriphClkInitStruct) != HAL_OK)
 {
 Error_Handler();
 }
}
 

What is the workaround?

This topic has been closed for replies.

9 replies

TDK
March 21, 2022

Attaching an IOC that replicates the problem would be helpful. Might be a bug, might be some other explanation.

Which ADC? Which chip?

"If you feel a post has answered your question, please click ""Accept as Solution""."
GerHebert
GerHebertAuthor
Associate II
March 22, 2022

I attach the ioc.

Chip: STM32H750VBTx

Since 6.5.0 (FW 1.10), all ADC's into the chip do not have their clock configured correctly.

With CubeMX 6.4.0 (FW 1.9), the To ADC was blue and ADC's clock were configured correctly.

0693W00000KdTrwQAF.png

GerHebert
GerHebertAuthor
Associate II
March 22, 2022

I just started a project from scratch with STM32H750VBTx, I haven't been able to activate ADC clock yet. Pretty easy to reproduce...

Amel NASRI
ST Technical Moderator
March 23, 2022

Hi @GerHebert​ ,

This seems to be the same issue as reported in the following 2 questions:

Internal ticket number: 124251 (This is an internal tracking number and is not accessible or usable by customers).

@Khouloud OTHMAN​ can confirm or clarify more this issue.

-Amel

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.
Khouloud OTHMAN
Associate
March 24, 2022

Hi @GerHebert​ ,

You're right, the issue is reproduced and confirmed.

Actually, a regression was detected with the latest STM32CubeMX 6.5.0 version: Clock Prescaler parameter removal from the GUI and the non-activation of ADC Clock Mux although the ADC is configured.

As mentioned by @Amel NASRI​ , this misbehavior was already reported internally to be fixed as soon as possible.

I'll keep you posted with the updates.

Sorry for any inconvenience that this may cause.

Khouloud.

R Piacenzia
Associate II
April 1, 2022

I have the same issue. Is there an ETA for this fix?

TDK
April 1, 2022

Historically, it has been several months between CubeMX releases, and one just came out recently.

"If you feel a post has answered your question, please click ""Accept as Solution""."
Tim Goll
Associate II
April 21, 2022

36 days have passed and this is still broken, wow. I just spent two days trying to figure out why my project is suddenly broken.

For anyone wondering: downgrade to version 1.7.0. You have to change you ioc file version though:0693W00000LydZsQAJ.png

ADunc.1
Senior
June 13, 2022

I just came across this problem... Any idea when a fix will be released?