Skip to main content
GOh.4
Visitor II
Mar 17, 2022 1:21 AM UTC
Solved

STM32H755ZI-Q CubeMX Does not generate ADC clocks

Hello,

I have recently encountered an issue after updating STM32CubeMX to the most recent version 6.5.0.

The said version seem to have missing ADC "Clock Prescaler" in the configuration menu and ADC clock generation is locked disabled in the "Clock Configuration" menu even when ADC is set enabled.

The issues are gone when downgraded to 6.4.0.

Please have a look on this issue.

Thank you

Board: Nucleo STM32H755ZI-Q

Firmware: STM32Cube FW_H7 V1.10.0

Image 1: No "Clock Prescaler" menu in the ADC configuration menu

0693W00000Kcvz2QAB.pngImage2: ADC clock configuration is locked disabled even when ADC1 is set enabled.

0693W00000KcvzWQAR.png 

This topic has been closed for replies.
Sara BEN HADJ YAHYA
ST Technical Moderator
Mar 17, 2022 7:49 AM UTC

Hello @GOh.4​ ,

Thanks for your feedback,

This is a known issue and it is already reported to the dev team to be fixed. I will keep you posted with the updates.

Internal ticket number: 124641 (This is an internal tracking number and is not accessible or usable by customers).

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.

2 replies

Sara BEN HADJ YAHYA
ST Technical Moderator
Mar 17, 2022 7:49 AM UTC

Hello @GOh.4​ ,

Thanks for your feedback,

This is a known issue and it is already reported to the dev team to be fixed. I will keep you posted with the updates.

Internal ticket number: 124641 (This is an internal tracking number and is not accessible or usable by customers).

If your issue is solved, please close this post by clicking the "Select as Best" button. This will help other members of the community find this response more quickly :)

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.
Sara BEN HADJ YAHYA
ST Technical Moderator
Jun 29, 2022 3:08 PM UTC

Hello @GOh.4​ ,

This issue is fixed in STM32CubeMX latest release.

V6.6.0 is now available under this Link.

Thanks for your contribution.

Sara.

In order to give better visibility on the answered topics, please click on 'Best answer' on the reply which solved your issue or answered your question.