Skip to main content
DSchä.2
Visitor II
Mar 30, 2022 8:06 AM UTC
Question

CubeProgrammer with J-Link

Is it planned that in the future the cube programmer will also work with the j-link like the cubeIDE?

This topic has been closed for replies.

5 replies

Pavel A.
Mar 30, 2022 2:20 PM UTC

+1

We have one board that cannot work with ST-LINK because of design defect (to be fixed later);

It works with J-LINK in JTAG mode.

CubeIDE can use J-LINK for loading and debugging the program but I really miss full CubeProgrammer functionality - option bytes etc, that is hard with J-LINK software.

ASatt
Associate II
Apr 16, 2024 1:33 PM UTC

Hi Pavel,

 

Can you please look into the following link. STM32CubeProgrammer & STM32CubeMonitor support SEGGER's J-Links

And please let me know which version of the cube programmer. 

 

kind regards,

Abdul

 

Houda GHABRI
ST Employee
Apr 12, 2022 9:59 AM UTC

Hi @DS.5chäfer​ ,@Pavel A.​ ​ 

I see your point and will bring it up to the STM32CubeProgrammer team but to be honest it won't be treated in short term.

 Internal ticket number:  126303 (PS: This is an internal tracking number and is not accessible or usable by customers). 

Houda

Associate
Mar 24, 2023 5:05 PM UTC

Oh my gosh! I'd LOVE to use my J-Trace Pro with the STM32CubeProgrammer software.

AScha.3
Super User
Apr 16, 2024 2:07 PM UTC
If you feel a post has answered your question, please click on " Best Answer ".