Question
RM0091 - ADC chapter not very clear
Hi,
The RM0091 rev 9 has some contradictions and typos in the ADC chapter.
- on page 234, 13.4.4 says that the registers IER, CFGRi, SMPR, TR, CHSELR and CCR must be configured only after ADEN has been set (and presumably that ADRDY is also set).
- However in section 13.5.2, it is said that the RES bits in CFGR1 must only be changed when ADEN = 0.
- So which one of the above should I follow ?
- on page 252, for calculating the Vdda value, a value of .3V is mentionned twice (I presume 3.3V, as written in the next formula).
Best regards.