Skip to main content
MPehi.1
Associate II
March 5, 2021
Question

Correct settings for FDCAN in CAN2.0 Mode using a ST G431KB Microcontroller

  • March 5, 2021
  • 1 reply
  • 1854 views

Dear ST Community,

I am trying to use the FDCAN peripheral of the G431KB STMicroelectronics Microcontroller.

It is a project requirement that the FDCAN is used in CAN 2.0 mode (FDCAN_CLASSIC_CAN). FDCAN is backwards-compatible so thus far there's no issues.

I am having difficulties setting up the FDCAN in the required setting in the STM32CubeIDE program.

The `HAL_FDCAN_Start()` function returns `HAL_OK` . 

The `HAL_FDCAN_AddMessageToTxFifoQ()` function, however, returns the `HAL_FDCAN_ERROR_FIFO_FULL` error code.

I initialize the FDCAN as usual:

can_filterConfig.IdType = FDCAN_STANDARD_ID;
 can_filterConfig.FilterIndex = 0;
 can_filterConfig.FilterType = FDCAN_FILTER_MASK;
 can_filterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
 can_filterConfig.FilterID1 = 0x000;
 can_filterConfig.FilterID2 = 0x000;
 
 	if( HAL_OK != HAL_FDCAN_ConfigFilter(&hfdcan1, &can_filterConfig) )
 	{
 		/* Filter configuration Error */
 		Error_Handler();
 	}
 
 	/* Activate the usage of interrupts */
 	if( HAL_OK != HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE | FDCAN_IT_TX_FIFO_EMPTY, FDCAN_TX_BUFFER0 | FDCAN_TX_BUFFER1 | FDCAN_TX_BUFFER2) )
 	{
 		/* Filter configuration Error */
 		Error_Handler();
 	}
 
 	/* Start the peripheral */
 	if( HAL_OK != HAL_FDCAN_Start(&hfdcan1) )
 	{
 		/* Filter configuration Error */
 		Error_Handler();
 	}

In the interrupt service routine of the GPIOs (`HAL_GPIO_EXTI_Callback()`) I call a function that sends the CAN messages. 

can_txHeader.Identifier = 0x007;
	can_txHeader.IdType = FDCAN_STANDARD_ID; 		/* 11 bit */
	can_txHeader.TxFrameType = FDCAN_DATA_FRAME;
	can_txHeader.DataLength = FDCAN_DLC_BYTES_4;
	can_txHeader.ErrorStateIndicator = FDCAN_ESI_PASSIVE;
	can_txHeader.BitRateSwitch = FDCAN_BRS_OFF;
	can_txHeader.FDFormat = FDCAN_CLASSIC_CAN;		/* Not CAN-FD */
	can_txHeader.TxEventFifoControl = FDCAN_STORE_TX_EVENTS;
	can_txHeader.MessageMarker = 0x00;
 
	if(HAL_OK != HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &can_txHeader, txData))
	{
		i8_error = 1;
	}
 
	return i8_error;

Because of the above mentioned `HAL_FDCAN_ERROR_FIFO_FULL` error code, the variable `i8_error` returns `1`.

Am I doing something wrong during the CAN-setup? 

What could be the cause of the `HAL_FDCAN_ERROR_FIFO_FULL` error?

I do understand what it means for the FIFO to be full.

So I suppose what I am asking is - how can I empty the FIFO? Doesn't the CAN peripheral take care of sending the messages on the FIFO in the background?

I have tried debugging with no avail thus far.

If you can provide me with some program examples or sources of information, I would be very grateful!

Any help is highly appreciated. Should more information be required, I am able to provide more.

Kind regards,

Mihail

This topic has been closed for replies.

1 reply

SKacp.1
Associate
March 5, 2021