Skip to main content
TheGuyFromTheHills
Associate
May 26, 2020
Solved

get no coomunication via FDCAN1 on STM32G431RB NUCLEO board

  • May 26, 2020
  • 1 reply
  • 3605 views

0693W000001pQcvQAE.pngHi,

I try to send data via CAN from the nucleo board to a USB-to-CAN device (peakCAN).

I configured PA12 and PA11 as FDCAN1_TX and FDCAN1_RX. I measured pin 12 and pin 14 on the CN10 connector with a salea logic device, but got no valid frame. Pin 12 stays high (3.3V) and pin 14 remains low (0V).

I also tried to change the PLL-frequency for the CAN peripheral to 40MHz as mentioned in some other posts (seen in the snippets below) - but it has the same effect like my implementation with 36MHz...

Can anyone help me with this problem? Thanks a lot...

static void MX_FDCAN1_Init(void)
{
 
 /* USER CODE BEGIN FDCAN1_Init 0 */
 
 /* USER CODE END FDCAN1_Init 0 */
 
 /* USER CODE BEGIN FDCAN1_Init 1 */
 
 /* USER CODE END FDCAN1_Init 1 */
 hfdcan1.Instance = FDCAN1;
 hfdcan1.Init.ClockDivider = FDCAN_CLOCK_DIV1;
 hfdcan1.Init.FrameFormat = FDCAN_FRAME_CLASSIC;
 hfdcan1.Init.Mode = FDCAN_MODE_NORMAL;
 hfdcan1.Init.AutoRetransmission = DISABLE;
 hfdcan1.Init.TransmitPause = DISABLE;
 hfdcan1.Init.ProtocolException = DISABLE;
 hfdcan1.Init.NominalPrescaler = 4;
 hfdcan1.Init.NominalSyncJumpWidth = 8;
 hfdcan1.Init.NominalTimeSeg1 = 31;
 hfdcan1.Init.NominalTimeSeg2 = 8;
 hfdcan1.Init.DataPrescaler = 1;
 hfdcan1.Init.DataSyncJumpWidth = 1;
 hfdcan1.Init.DataTimeSeg1 = 1;
 hfdcan1.Init.DataTimeSeg2 = 1;
 hfdcan1.Init.StdFiltersNbr = 0;
 hfdcan1.Init.ExtFiltersNbr = 0;
 hfdcan1.Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
 if (HAL_FDCAN_Init(&hfdcan1) != HAL_OK)
 {
 Error_Handler();
 }
 /* USER CODE BEGIN FDCAN1_Init 2 */
 
 /* USER CODE END FDCAN1_Init 2 */
 
}
void FDCAN_config(void)
{
	FDCAN_FilterTypeDef sFilterConfig;
 
	sFilterConfig.IdType = FDCAN_STANDARD_ID;
	sFilterConfig.FilterIndex = 0;
	sFilterConfig.FilterType = FDCAN_FILTER_MASK;
	sFilterConfig.FilterConfig = FDCAN_FILTER_TO_RXFIFO0;
	sFilterConfig.FilterID1 = 0x000;
	sFilterConfig.FilterID2 = 0x7FF;
 
	if(HAL_FDCAN_ConfigFilter(&hfdcan1, &sFilterConfig) != HAL_OK)
	{
		Error_Handler();
	}
 
	if(HAL_FDCAN_ConfigGlobalFilter(&hfdcan1, FDCAN_REJECT, FDCAN_REJECT, FDCAN_FILTER_REMOTE, FDCAN_FILTER_REMOTE) != HAL_OK)
	{
		Error_Handler();
	}
 
	if(HAL_FDCAN_Start(&hfdcan1) != HAL_OK)
	{
		Error_Handler();
	}
 
	if(HAL_FDCAN_ActivateNotification(&hfdcan1, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0) != HAL_OK)
	{
		Error_Handler();
	}
 
	TxHeader.Identifier = 0x123;
	TxHeader.IdType = FDCAN_STANDARD_ID;
	TxHeader.TxFrameType = FDCAN_DATA_FRAME;
	TxHeader.DataLength = FDCAN_DLC_BYTES_8;
	TxHeader.ErrorStateIndicator = FDCAN_ESI_ACTIVE;
	TxHeader.BitRateSwitch = FDCAN_BRS_OFF;
	TxHeader.FDFormat = FDCAN_CLASSIC_CAN;
	TxHeader.TxEventFifoControl = FDCAN_NO_TX_EVENTS;
	TxHeader.MessageMarker = 0;
}
int main(void)
{
 /* USER CODE BEGIN 1 */
 
 /* USER CODE END 1 */
 
 /* MCU Configuration--------------------------------------------------------*/
 
 /* Reset of all peripherals, Initializes the Flash interface and the Systick. */
 HAL_Init();
 
 /* USER CODE BEGIN Init */
 
 /* USER CODE END Init */
 
 /* Configure the system clock */
 SystemClock_Config();
 
 /* USER CODE BEGIN SysInit */
 
 /* USER CODE END SysInit */
 
 /* Initialize all configured peripherals */
 MX_GPIO_Init();
 MX_LPUART1_UART_Init();
 MX_FDCAN1_Init();
 /* USER CODE BEGIN 2 */
 
 FDCAN_config();
 
 /* USER CODE END 2 */
 
 /* Infinite loop */
 /* USER CODE BEGIN WHILE */
 while (1)
 {
	 myCanState = HAL_FDCAN_GetState(&hfdcan1);
	 HAL_GPIO_TogglePin(GPIOA, GPIO_PIN_5);
	 HAL_Delay(500);
	 myState = HAL_FDCAN_AddMessageToTxFifoQ(&hfdcan1, &TxHeader, &myTxData[0]);
 
 /* USER CODE END WHILE */
 
 /* USER CODE BEGIN 3 */
 }
 /* USER CODE END 3 */
}

This topic has been closed for replies.
Best answer by SKacp.1

Hello,

Please se my code for Nucleo-64 STM32G474RE. Its works.

Baudrate for CAN I set on 1000 kbit/s.

Clock for FDCAN is set on 80 MHz.

Please check settings for the instance "hfdcan1" and the system clock configuration.

I check this example with UCANDevices https://ucandevices.github.io/uccb.html

Best regards,

Slawek

1 reply

SKacp.1
SKacp.1Best answer
Associate
May 26, 2020

Hello,

Please se my code for Nucleo-64 STM32G474RE. Its works.

Baudrate for CAN I set on 1000 kbit/s.

Clock for FDCAN is set on 80 MHz.

Please check settings for the instance "hfdcan1" and the system clock configuration.

I check this example with UCANDevices https://ucandevices.github.io/uccb.html

Best regards,

Slawek