Question
STM32 on 1.8V - I2C with 3.5 PullUp
Hello,
my STM32 is running with 1.8V and is connected via I2C to another chip. The I2C has an level of 3.5V (connected via pullup to 3.5). I now have communication problems. Is there any limitation for maximum voltage for the high level of I2C on STM32 so that that could be the reason for not working?
Best regards
Fabian