Skip to main content
BHure.1
Associate III
October 19, 2020
Question

H750 Discovery board - STLINK v3

Hello, Got a stm32H750B discovery board and it kills me as i don't fully understand.

I managed to understand a bit with the help of clive, as right now when i try to connect with STLINk v2 on the SWD connection i get a STM32F72X chip recognised (not the board itself).

Is it possible to flash this chip in order to make it the board functional again?

Thanks,

Bogdan

This topic has been closed for replies.

5 replies

Tesla DeLorean
Guru
October 19, 2020
Tips, Buy me a coffee, or three.. PayPal Venmo (See Profile) Up vote any posts that you find helpful, it shows what's working..
BHure.1
BHure.1Author
Associate III
October 20, 2020

The F723 seems to be empty.

PC does not recognise the STLINK. when i plug the usb inside the STLK connector, there is no activity - the LD4 should be lighted, but it is dead.

Uwe Bonnes
Chief
October 20, 2020

Did you perhaps not remove JP3 and the F723 is still under reset?

BHure.1
BHure.1Author
Associate III
October 20, 2020

No, JP3 is unset.

Tried to reset F723 by setting JP3. It is under reset, but still no difference :(.

It is very likely i removed the firmware on F723. Don't know how i managed to do that. Tried several times to force H7 to reset bootloader, however it does not work.

Uwe Bonnes
Chief
October 20, 2020

I am quite sure the STLinkV3 bootloader is RDP1 protected. From V37 on, the SWD access to the F723 is closed. Try to access the F723 via CN5 with another adapter.

However I guess you somehow applied voltage above VCC of some F723 pin and that killed the F723...