2020-05-31 6:06 PM
[ The text uses a translation tool. ]
Flash size is the default and no more programs can be loaded.
environment
Windows10 + STM32CubeMX + ST-Link2
************** Console log
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
ST-LINK SN : 53FF6D064882505226101587
ST-LINK FW : V2J36S7
Voltage : 3.23V
SWD freq : 4000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x436
Device name : STM32L15xxD/STM32L162xD
Flash size : 128 KBytes (default)
Device type : MCU
Device CPU : Cortex-M3
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a20796.srec
File : ST-LINK_GDB_server_a20796.srec
Size : 137888 Bytes
Address : 0x08010000
Erasing memory corresponding to segment 0:
Error: Operation exceeds memory limits
Error: failed to erase memory
Encountered Error when opening C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.3.0.202002181050\tools\bin\STM32_Programmer_CLI.exe
Error in STM32CubeProgrammer
Debugger connection lost.
Shutting down...
*************
I'm using an STM2L151DTx, so there's plenty of flush
Why is it [Flash size: 128 KBytes (default)]?
The STM32 ST-LINK Utility can be recognized and written normally.
Am I doing something wrong?
2020-07-03 3:09 PM
I am seeing the same problem and think I've narrowed it down a bit.
@ST Please review!!!
I have two prototype boards, both are STM32L151RCT6A
Board 1 (device id 0x427):
C:\Users\Dave>"C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ST-LINK_CLI.exe" -c
STM32 ST-LINK CLI v3.5.0.0
STM32 ST-LINK Command Line Interface
ST-LINK SN: 49FF70064986555549352587
ST-LINK Firmware version: V2J35S7
Connected via SWD.
SWD Frequency = 4000K.
Target voltage = 2.9 V
Connection mode: Normal
Reset mode: Hardware reset
Device ID: 0x427
Device flash Size: 256 Kbytes
Device family: STM32L100xC/L15xxC/L162xC
C:\Users\Dave>C:\Users\Dave>"C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=SWD
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
ST-LINK SN : 49FF70064986555549352587
ST-LINK FW : V2J35S7
Voltage : 2.90V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x427
Device name : STM32L100xC/STM32L15xxC/STM32L162xC
Flash size : 256 KBytes
Device type : MCU
Device CPU : Cortex-M3
C:\Users\Dave>So far so good... Both STLink utility and STM32CubeProgrammer report device ID 0x427 and correct flash size of 256kbytes
Board 2 (device id 0x436):
C:\Users\Dave>"C:\Program Files (x86)\STMicroelectronics\STM32 ST-LINK Utility\ST-LINK Utility\ST-LINK_CLI.exe" -c
STM32 ST-LINK CLI v3.5.0.0
STM32 ST-LINK Command Line Interface
ST-LINK SN: 49FF70064986555549352587
ST-LINK Firmware version: V2J35S7
Connected via SWD.
SWD Frequency = 4000K.
Target voltage = 2.9 V
Connection mode: Normal
Reset mode: Hardware reset
Device ID: 0x436
Device flash Size: 256 Kbytes
Device family: STM32L15xxC-xxD/L162xC-xD
C:\Users\Dave>C:\Users\Dave>"C:\Program Files (x86)\STMicroelectronics\STM32Cube\STM32CubeProgrammer\bin\STM32_Programmer_CLI.exe" -c port=SWD
-------------------------------------------------------------------
STM32CubeProgrammer v2.4.0
-------------------------------------------------------------------
ST-LINK SN : 49FF70064986555549352587
ST-LINK FW : V2J35S7
Voltage : 2.90V
SWD freq : 4000 KHz
Connect mode: Normal
Reset mode : Software reset
Device ID : 0x436
Device name : STM32L15xxD/STM32L162xD
Flash size : 1 KBytes
Device type : MCU
Device CPU : Cortex-M3
C:\Users\Dave>Problem: on board 2, STlink utility reports 256kb, and STM32cube reports 1kb.
I see the same 1kb in the GUI version (STM32CubeProgrammer.exe).
According to reference manual RM0038 Rev 16:
Bits 15:0 F_SIZE: Flash memory size
For DEV_ID = 0x416 or 0x427 or 0x429 or 0x437, this field value indicates the Flash memory size of the device in Kbytes.
Example: 0x0080 = 128 Kbytes.
For DEV_ID = 0x436, the field value can be ‘0’ or ‘1’, with ‘0’ for 384 Kbytes and ‘1’ for 256 Kbytes. Note: For DEV_ID = 0x429, only LSB part of F_SIZE: F_SIZE[7:0] is valid. The MSB part F_SIZE[15:8] is reserved and must be ignored.
When I run from atollic 9.0.1 in debug mode and view register *0x1FF800CC, i see the value 0x0001. So I think this should be reported as 256kb, and ST-LINK_CLI.exe seems to handle this correctly, but STM32_Programmer_CLI.exe doesnt.
Could this be a bug in STM32_Programmer_CLI.exe, which is ignoring the special case of DEV_ID=0x436, and treating *0x1FF800CC=1 as meaning 1kbyte?
Effect: cannot erase or program this device using STM32CubeProgrammer.exe or STM32_Programmer_CLI.exe.
Workaround: use ST-LINK_CLI.exe or the gdb debugger built into the IDE rather than STM32CubeProgrammer.
Happy to provide more info to help if needed.
2020-11-23 7:20 AM
Is there a solution to this problem yet?
I have a similar problem. I am using STM32L152ZCT6 with STM32CubeIDE.
@clive1 , et. al
2020-11-23 9:03 AM
I'm not responsible for any of this...
Yes, there does some to be a recurrent issue with the correct identification of flash size by STM32 Cube Programmer, and it may well have to do with whether it reads the FLASH_SIZE as an 8 or 16-bit wide value.
2020-11-23 9:06 AM
@Nawres GHARBI @Imen DAHMEN @Amel NASRI
2020-11-23 9:14 AM
Thanks. I will await response from those you mentioned.
2020-11-23 11:11 AM
I don't think the issue or 8 or 16bits, its that (as per the datasheet) device ID=0x436 is a special case which means "ignore all other rules" and interpret (uint_16)*0x1FF800CC as...
0: 384k
1: 256k
2-65535: (undefined I assume)
If they forgot to put in this logic, then the 'standard' code would just multiply the value by 1k resulting in ...
0: 0k
1: 1k
2020-11-24 12:27 AM
Thanks. I just understood your previous response properly.
2020-11-25 2:42 AM
Hello All, problem is already under fix
will be delivered for the next release, sorry for the disturbance
2021-06-03 1:04 AM
Hello,
environment
Windows 10 + STM32CubeIDE(v1.6.1) + ST-Link2
Windows 10 + STM32CubeProgrammer(v2.7.0) + ST-Link2
Windows 10 + STM32 ST-LINK Utility(4.6.0) + ST-Link2
My Microcontroller: Stm32l151RD flash size 384 Kbytes, 48 Kbytes ram, Package LQFP64.
I have same problems. I cannot send my code. I tried to use STM32CubeIDE and STM32CubeProgrammer. 2 programs seen 128kB flash size. Why is it [Flash size: 128 Kbytes (default)]? How can I change flash size 128kB default value?
Also, I can send my code when I try to send with STM32 ST-LINK Utility. Because STM32 ST-LINK Utility can recognize the 384kB flash size correctly.
*************Screenshot from STM32CubeProgrammer*************
*************
I am waiting your solutions @Nawres GHARBI @Imen DAHMEN @Amel NASRI.
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.