Skip to main content
高健一.1
Visitor II
Jun 1, 2020 1:06 AM UTC
Question

STM32CubeMX can't recognize the flash size correctly and the debugger won't start

[ The text uses a translation tool. ]

Flash size is the default and no more programs can be loaded.

environment

Windows10 + STM32CubeMX + ST-Link2

************** Console log

     -------------------------------------------------------------------

                      STM32CubeProgrammer v2.4.0                 

     -------------------------------------------------------------------

ST-LINK SN : 53FF6D064882505226101587

ST-LINK FW : V2J36S7

Voltage    : 3.23V

SWD freq   : 4000 KHz

Connect mode: Under Reset

Reset mode : Hardware reset

Device ID  : 0x436

Device name : STM32L15xxD/STM32L162xD

Flash size : 128 KBytes (default)

Device type : MCU

Device CPU : Cortex-M3

Memory Programming ...

Opening and parsing file: ST-LINK_GDB_server_a20796.srec

 File         : ST-LINK_GDB_server_a20796.srec

 Size         : 137888 Bytes

 Address      : 0x08010000

Erasing memory corresponding to segment 0:

Error: Operation exceeds memory limits

Error: failed to erase memory

Encountered Error when opening C:\ST\STM32CubeIDE_1.3.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_1.3.0.202002181050\tools\bin\STM32_Programmer_CLI.exe

Error in STM32CubeProgrammer

Debugger connection lost.

Shutting down...

*************

I'm using an STM2L151DTx, so there's plenty of flush

Why is it [Flash size: 128 KBytes (default)]?

The STM32 ST-LINK Utility can be recognized and written normally.

Am I doing something wrong?

This topic has been closed for replies.

21 replies

herca.1
Associate II
Aug 17, 2021 11:43 AM UTC

Hello,

Using 2.8.0 and using STM32L15xx microcontroller

This is the output of Cube Programmer. Verbosity level 3. Is this also fixed for CubeMX IDE, I want to be able to debug my software.

 14:40:51:303 :  Size     : 263956 Bytes

 14:40:51:303 :  Address    : 0x08000000 

 14:40:51:303 : Erasing Segment <0> Address <0x08000000> Size <263956>Bytes

 14:40:51:303 : Erasing memory corresponding to segment 0:

 14:40:51:303 : Memory erase...

 14:40:51:322 : halt ap 0 

 14:40:51:322 : w ap 0 reg 15 PC  (0x20000000)  

 14:40:51:331 : w ap 0 reg 17 MSP (0x20000500)  

 14:40:51:331 : w ap 0 reg 16 xPSR (0x01000000)  

 14:40:51:336 : w ap 0 @0x20000E20 0x00000200 bytes Data 0x00000000

 14:40:51:336 : w ap 0 @0x20000000 0x00000004 bytes Data 0x0000BE00

 14:40:51:362 : w ap 0 @0x20000004 0x000009EC bytes Data 0xF8DFB580

 14:40:51:363 : Error: Operation exceeds memory limits

 14:40:51:381 : Error: failed to erase memory

herca.1
Associate II
Sep 22, 2021 2:37 PM UTC

WHEN WILL YOU FIX THIS ISSUE????????????????????????????????