Skip to main content
MK S.1
Visitor II
February 14, 2020
Solved

Hi, i am using stm32IDE if i entering into debug mode getting this error please help me to crack this. Failed to bind to port 61234, error code -1: No error Failure starting GDB server: TCP port 61234 not available.

  • February 14, 2020
  • 19 replies
  • 23599 views

..

This topic has been closed for replies.
Best answer by KFuhr.1

I could fix it by restarting my PC. apparently the GDB server needed a restart

19 replies

MKiri.1
Visitor II
May 22, 2020

me to

CubeIDE win10

KFuhr.1
Visitor II
October 14, 2020

Me too

It just happend and I don't know how.

warm38
Associate III
October 14, 2020

downloaded 1.4.0

installed it

ran 1.4.0

compiled latest program

0 errors 0 warnings

Check for upgrade

upgraded to 1.4.2

Compiled current program

0 errors 0 warnings

Click Debug

LED turned red

No other indication

Help -> ST Link Upgrade

refresh list

open in upgrade mode

upgrade successful

LED still red

COM port shows up, but teraterm cannot connect to it

Click Debug

and get the error message

Error in final launch sequence:

Failed to start GDB server

Failed to start GDB server

Error in initializing ST-LINK device.

Reason: (-1) Unknown. Please check power and cabling to target.

look at comsole

STMicroelectronics ST-LINK GDB server. Version 5.6.0

Copyright (c) 2020, STMicroelectronics. All rights reserved.

Starting server with the following options:

       Persistent Mode           : Disabled

       Logging Level             : 1

       Listen Port Number        : 61234

       Status Refresh Delay      : 15s

       Verbose Mode              : Disabled

       SWD Debug                 : Enabled

       InitWhile                 : Enabled

Failed to bind to port 61234, error code -1: Result too large

Failure starting GDB server: TCP port 61234 not available.

Try again to debug

0 errors 0 warnings

pop up saying newer version of ST Link available Upgrade? YES

Open in upgrade mode

Unexpected error during opening (1)

Device 0672FF534953867067064047 not found. No device connected.

this is on two Nucleo-STM32F401RE boards

How do I fix both boards so they can communicate again.

KFuhr.1
KFuhr.1Best answer
Visitor II
October 14, 2020

I could fix it by restarting my PC. apparently the GDB server needed a restart

warm38
Associate III
October 14, 2020

I tried restarting my PC and it WORKED. I guess Windows doesn't like being up for 2 months. :)

Thanks for the suggestion.

GOtté.1
Visitor II
January 15, 2021

I encountered the same. The problem was that the link server was still running in the background. I used the Task Manager to kill it, restarted STM32CubeIDE, and it worked again without the need of rebooting my PC.

C:\Program Files (x86)\STMicroelectronics\stlink_server\stlinkserver.exe

BareKnuckle
Visitor II
February 15, 2021

Hi all,

Instead of restarting the PC, connecting to St board or MCU with ST-Link Utility and erasing the chip before loading the code helps too.

Kepo
Visitor II
March 30, 2021

Restart the PC works fine after an upgrade.

Seunghun Kim
Visitor II
September 15, 2021

Changing port number might help. I changed the port number of GDB server from 61234 to 41234 in debug configurations, and it worked without rebooting my computer.

Garnett.Robert
Senior III
November 21, 2021

Hi,

This worked for me.

The error is strange and I am able to use the ST Programmer program with the 61234, and you can even do an upgrade of the ST Link firmware, but it won't connect under debug unless I change the port.

Thank's

Rob

KShen.1
Associate II
January 11, 2022

It works. I even try to reinstall the ide and programmer before that, but still cannot get it work...