Skip to main content
Till Rachow
Associate III
Aug 2, 2018 2:41 PM UTC
Question

STM32CubeMX Mac updater does not work

Hi,

whenever I try to run the CubeMX updater on MacOS, using sudo, the update will fail with:

" Updater cannot write on Software Folder. It's probably due to a bad Acces Privilege."

I tried to give everyone, admin and me the right to read and write the folder and the app itself. No success!

Anybody knows how to make it work?

Thanks

    This topic has been closed for replies.

    13 replies

    Khouloud GARSI
    ST Employee
    Aug 10, 2018 3:13 PM UTC

    Hi @Till Rachow​ ,

    Your seen behavior is reported to our CubeMX team.

    We will update you ASAP.

    Khouloud.

    Mohamed Mansouri
    Visitor II
    Aug 17, 2018 8:06 AM UTC

    Hi @Till Rachow,

    Thanks for your feedback,

    Unfortunately, I have not been able to reproduce this issue. Can you please help us to solve this by:

    • Indicate your CubeMX version.
    • share your .log file ( you will find it under this directory: Users/..../.stm32cubemx/).
    • inform us about the access mode for your "repository" folder: can you please apply ls -ll for "STM32Cube" folder (/Users/.../STM32Cube/).

    Thanks in advance for helping to complete this thread,

    Best regards,

    Mohamed

    Till Rachow
    Associate III
    Aug 20, 2018 8:47 AM UTC

    Hi @Mohamed Mansouri​ ,

    I have CubeMX Version 4.26.1

    -ll gives me : drwxr-xr-x 11 username staff 352 2 Aug 16:57 Repository

    Thanks,

    Till

    KOstr
    Visitor II
    Aug 23, 2018 7:02 AM UTC

    Have the same problem with the V4.19.0.

    KOstr
    Visitor II
    Aug 23, 2018 7:03 AM UTC

    On Win7 64Bit Ultimate

    Mohamed Mansouri
    Visitor II
    Aug 30, 2018 3:31 PM UTC

    Hi @Till Rachow​,

    Unfortunately, i couldn't reproduce this issue. Installing CubeMX using sudo and under application folder, I succeeded to launch the updater without any problems.

    Can you please tell us if you are using Proxy or WiFi for internet connection.

    Can you also, please, give more details about the steps to reproduce this bug (how did you launch the updater, when exactly did the pop up message occur).

    Try to delete this two folders: .stm32cubemx and .stmcufinder ( you find it under /Users/tilljascharachow/) and check if there are generated again when you restart CubeMX.

    Best regards,

    Mohamed

    sqnewton
    Visitor II
    Sep 21, 2018 4:59 PM UTC

    I am having the same problem with Mac. Plus funny that the error message has some typos ("It's pobably" and "Acces". Anyone has been successful with this? Plus installing the 32L476 package doesn't work well either... I wish ST would pay more attention to their development community.

    Derry Tannama
    Visitor II
    Oct 28, 2018 5:39 PM UTC

    Hi when i update CubeMX Version 4.27, i have same problem with you

    for solving this, i just run MX Cube icon in dekstop with 'Run As Administrator' and it works normally

    Maybe it can works with you

    Thanks

    Associate II
    Apr 26, 2019 8:38 PM UTC

    I have the same problem. Running Mojave 10.14.4, STM32CubeMX Version 4.22.1 (STM32Cube V1.0) .

    I launch the app with sudo: $ sudo open -a /Applications/STMicroelectronics/STM32CubeMX.app

    I select menu Help>Check For Updates

    I am offered MX.5.2.0 and I check this box, then click on Install Now

    FIles download and a dialog appears "You need to restart STM32CubeMX with Administrator privileges to terminate installation"; I click OK

    I close the Update Manager window

    I File>Exit from the main window

    I launch the app with the same sudo (see above)

    The update always, always fails claiming error "Software cannot write on Software Folder."

    ALiss
    Associate II
    Sep 24, 2019 11:29 AM UTC

    Hey guys, I had the same problem but just now solved it. If anyone is still wondering how to solve this issue I did it the following way:

    • Find the STM32CubeMX file in your /Applications folder
    • Right-click -> "Show package contents"
    • Locate STM32CubeMX in Contents/Resources/
    • Open terminal and use "sudo USER/Applications/STMicroelectronics/STM32CubeMX.app/Contents/Resources/STM32CubeMX"
      • tip: You can write "sudo " then drag n' drop the STM32CubeMX-file in package contents.
    • Go download the update in "Check for updates" in the cubeMX app. The program will tell you to restart.
    • Exit the program and start the program again as instructed above. Now it should be updating.

    JTera.1
    Visitor II
    Feb 5, 2020 7:12 AM UTC

    ALiss, thank you, This method worked for me. Cube 5.40 to 5.50 on macOS 10.15.3 Catalina.