Skip to main content
afinko
Associate II
April 28, 2010
Question

FAT file system on NAND flash

  • April 28, 2010
  • 16 replies
  • 4131 views
Posted on April 28, 2010 at 22:10

FAT file system on NAND flash

    This topic has been closed for replies.

    16 replies

    jdolera
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    Hi Afinko. Did you resolve your problem?

    afinko
    afinkoAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    NO, I did not :(

    rodolphe
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    Hello,

    what is the NAND Flash model or family ?

    Row and line addressing in Nand Flash are not always compatible between the ST Nand and the Atmel Nand.

    rodolphe
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    0690X00000602hkQAA.jpg

    hello,

    you must check that the address insertion in the read_block/write_block functions of your Nand Flash software driver comply with the address insertion format in the table above.

    regards.

    jdolera
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    I am using STM3210E-EVAL . Nand memory is NAND512W3A2CN6 from ST.

    Regards.

     

    afinko
    afinkoAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    > It's natural.

    > OS (Windows, Linux, MacOSX, etc) doesn't suppose that local storage is modified without OS intervention. If such an accident would occur, OS takes it as fault of the storage.

    >Unmount the media from the OS, before modifying it. And then, mount it again.

    Of course, I firstly unmonted the NAND from OS, then I mounted it in FatFs, created any file, unmounted from FatFs and mount to the OS.

    I can not see the created file even withouth unmonting (or with), when I want to read the file with FatFs.

    tsuneo
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    > If I am writing to the NAND by FatFS, no error occur, everything looks OK, but then in Mass Storage mode I can not find the file that was created by FatFS.

     

    It's natural.

    OS (Windows, Linux, MacOSX, etc) doesn't suppose that local storage is modified without OS intervention. If such an accident would occur, OS takes it as fault of the storage.

    Unmount the media from the OS, before modifying it. And then, mount it again.

    Tsuneo

    tsuneo
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    > Of course, I firstly unmonted the NAND from OS

    > If I use writing in FatFS several times, the another files on NAND start to be corrupted and at the end the whole FAT will fail

    It suggests that OS doesn't recognize unmount of the drive.

    How did you unmount the media from OS?

    To do it on the device side,

    Set RMB (removable) bit on the INQUIRY response.

    To notify media unmount to OS, the MSC device fails SCSI command from OS, except for INQUIRY. Usually OS puts TEST UNIT READY repeatedly. Fail on this command.

    OS may put many other SCSI commands while in unmount. Of course, device fails on these commands, too, while in unmount.

    - READ FORMAT CAPACITY

    - READ CAPACITY(10)

    - READ(10)

    - MODE SENSE(6)

    - PREVENT ALLOW MEDIUM REMOVAL

    etc.

    After the device fails in above commands, OS may put REQUEST SENSE. Return ''NOT READY - MEDIUM NOT PRESENT'' response, successfully.

    The point is that you have to wait for SCSI command (usually TEST UNIT READY) to fail, so that OS should know unmount certainly.

    There is another way which uses soft detach/attach of the device. But I don't recommend it, because Windows often fails on re-mount.

    Tsuneo

    afinko
    afinkoAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    > you must check that the address insertion in the read_block/write_block functions of your Nand Flash software driver comply with the address insertion format in the table above.

    The same read_block/write_block functions are used by Mass_Storage Mode, when it is used with Computer. And the Mass_Storage mode can write to the NAND.

    jdolera
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:49