Skip to main content
afinko
Associate II
April 28, 2010
Question

FAT file system on NAND flash

  • April 28, 2010
  • 16 replies
  • 4131 views
Posted on April 28, 2010 at 22:10

FAT file system on NAND flash

    This topic has been closed for replies.

    16 replies

    afinko
    afinkoAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    > It suggests that OS doesn't recognize unmount of the drive.

    > How did you unmount the media from OS?

    > To do it on the device side,

    > Set RMB (removable) bit on the INQUIRY response.

    > To notify media unmount to OS, the MSC device fails SCSI command from OS, except for INQUIRY. Usually OS puts TEST UNIT READY repeatedly. Fail on this command.

    > OS may put many other SCSI commands while in unmount. Of course, device fails on these commands, too, while in unmount.

    > - READ FORMAT CAPACITY

    > - READ CAPACITY(10)

    > - READ(10)

    > - MODE SENSE(6)

    > - PREVENT ALLOW MEDIUM REMOVAL

    > etc.

    > After the device fails in above commands, OS may put REQUEST SENSE. Return ''NOT READY - MEDIUM NOT PRESENT'' response, successfully.

    > The point is that you have to wait for SCSI command (usually TEST UNIT READY) to fail, so that OS should know unmount certainly.

    > There is another way which uses soft detach/attach of the device. But I don't recommend it, because Windows often fails on re-mount.

    > Tsuneo

    I tried to remove SD card to from the CORTEX board and put in the PC through SD card reader. I wrote some files on SD, and CORRETLY unmount the SD card by ''Safely Remove Hardware'' in Windows.

    Then I put the SD card to the CORTEX board, mount it with FatFs file system. I was able to read the files. Then I wrote some files with FatFs, unmount CORRECTLY the SD card with FatFs (according to the FatFs documentation).

    Then I removed the SD card from CORTEX board, connect to the PC through SD card readers, but the files that I wrote with CORTEX wasn't there.

    Do you really think that the problem is in unmounting the device?

    Afi

    dsolier
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    > Good news, I have done it.

    > We are missing something (still don't know what), but in your project, if you call your NAND_FAT function after Power off()  in MassStorageStart function instead of Demo_Init function , it will probably work.

    > There is something that MassStorage inits that is necessary to Write in the NANDFLASH

    Hi Afinko and Juan,

    YES, it works, but only if you plug USB cable. I did the same, but without the usb cable, and d

    I am finding out what from Mass_Storage_Start is required in order to be able to write to the NAND, and I think the problem is on the format of the file system.

    I'm using windows, and it format on FAT 32, but when I format with FatFS using f_mkfs, the format is on FAT16.

    Have you found what it's necessary to write in the Nand Flash correctly?

    Thanks

    David

    afinko
    afinkoAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    > Good news, I have done it.

    > We are missing something (still don't know what), but in your project, if you call your NAND_FAT function after Power off()  in MassStorageStart function instead of Demo_Init function , it will probably work.

    > There is something that MassStorage inits that is necessary to Write in the NANDFLASH

    Hi Juan,

    YES, It works in this case, You are the one ;)

    Thanks.

    I am going to find out what from Mass_Storage_Start is required in order to be able to write to the NAND.

    Afi

    jdolera
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    Good news, I have done it.

    We are missing something (still don't know what), but in your project, if you call your NAND_FAT function after Power off()  in MassStorageStart function instead of Demo_Init function , it will probably work.

    There is something that MassStorage inits that is necessary to Write in the NANDFLASH

    Regards.

    afinko
    afinkoAuthor
    Associate II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    > I am finding out what from Mass_Storage_Start is required in order to be able to write to the NAND, and I think the problem is on the format of the file system.

    > I'm using windows, and it format on FAT 32, but when I format with FatFS using f_mkfs, the format is on FAT16.

    > Have you found what it's necessary to write in the Nand Flash correctly?

    I spent several ours with this, unfortunately I didn't found what we are missing.

    It seems unstable even when the NAND_FAT function is called after Power off()  in MassStorageStart function.

    I do not have more time for resolving this issue. I do not need the NAND anymore.

    But I am very angry, that none from ST, who wrote the MASS_STORAGE functions, wont help us with this issue. I am pretty sure, that we are missing some stupid triviality.

    Afi
    dsolier
    Visitor II
    May 17, 2011
    Posted on May 17, 2011 at 13:49

    Sorry, I forgot to write all the post.

    >YES, it works, but only if you plug USB cable. I did the same, but without the usb cable, and doesn't work.