Question
Issues with Getting started with the STM32L152D-EVAL
Posted on October 13, 2014 at 06:12
Dear all,
I started to work on a STM32L152D-EVAL board. While I started to play around, I tried the demonstration firmware from the following link: http://www.st.com/web/en/catalog/tools/PF257910 I am using the IAR Compiler with I-Jet debugger. I am able to flash the board with new firmware, however nothing is showing up on the lcd, neither something happens when i press the joy stick as demonstrated.I thought the demonstration firmware should run out of the box. Am I missing something here?In particular I need examples related to the SPI interface for this board. Can someone please point me to the right samples for SPI on this board, which may work out of the box, so that I can then further customize the samples based on my needs? Thanks a lot. Regards, Pradeep #stm32l152d-eval-demonstratio-spi