Skip to main content
Associate
October 3, 2025
Question

VNQ9080 to controll auxiliary lights of my motorcycle

Hi all. I've made a dedicated PCB that should control auxiliary lights of my motorcycle. I use CANBUS information by MCP2515 module and using Arduino Nano digital output pins to directly control input pins of VNQ9080.

I assembled all elements on the PCB and tested the product by improvised wire connections to the connector holes. All worked as expected. I connected a connector ( a lot of curving copper wires to make it possible to install the device in a small plastic box) and installed all in the plastic box. I checked all connector points for eventual shorts with Fluke 179 ohmmeter. Everything looked well and I connected the product to my test wiring as before. What a disaster! My LED lights started blinking,... I found out that output pins delivered only about 3V instead of full battery voltage. I imagined that I have ruined the VNQ by applaying wrong voltage when tested with ohmmeter - Reverse Vcc is specified as 0.3V  

I prepared the second one. Assembled and connected the connector (a lot of work with curving connecting wires and soldering manually). This time no ohmmeter test. I connected the device. All looked well but I finaly find out that one output was broken - there are about 10V all the time with input low.

Do you have any idea what could be the reason for such problems?

Regards, Stojan

This topic has been closed for replies.

1 reply

Peter BENSCH
ST Technical Moderator
October 13, 2025

Welcome @stojank, to the community!

You asked almost the same question in this thread.

For better readability (not all community users can or want to read DOCX files), I took the trouble to insert the schematics and your layout as images.

Are you sure that the tab of the controller (labelled with a typo 8705 in the layout) is connected to GND, as no via is visible?

A reverse measurement with the ohmmeter does apply a voltage of a few volts to the device, but this is usually current-limited, so that the voltage collapses and should not destroy the device. However, a more accurate statement can only be made if the parameters of your ohmmeter are known. Assuming that the VNQ9080AJ was not soldered on upside down, I would assume that you handled it incorrectly and destroyed it, e.g. by not taking sufficient care with regard to ESD protection.

As for the permanently switched-on output, we can only speculate, as you have not specified exactly which one it is. If it is OUTPUT3, for example, you may have accidentally caused a short between pins 16 and 17.

Regards
/Peter

Nabor SMD elmentov s sliko schem.pngNabor SMD elmentov s sliko PCB.png

 

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.